Skip to main content
Remi Demers
Associate II
April 2, 2025
Solved

BlueNRG-LPS TIM to synchronize DMA transfert

  • April 2, 2025
  • 2 replies
  • 545 views

Hi,

I work with STEVAL-DB012VA, anf WISE-Studio over Linux. Starting from the peripheral exemple, I am trying to output a sequence of bits over GPIOB at a specific rate. To do this I am programming the DMA to transfert data from a buffer in memory to GPIOB->ODR and the DMAMUX to make the transfers clocked by TIM16 overflow.

The program compiles without warnings nor errors but nothing appears on the outputs.

Please look also to rf_driver_ll_dmamux.h. In the comments for LL_DMAMUX_SetRequestID, the list of possible values for "Request" parameter do not include LL_DMAMUX_REQ_TIM16_UP. This is what I used and it is probably why it do not works. But why? The TIM16 is supposed to be an option for synchronizing the DMA. Is it really possible?

See my code in the files main.c and app_main.c attached. Any clue?

Thanks,

Rémi

Best answer by Remi Demers

This was caused by missing clock on the timer. See this case where it is solved.

https://community.st.com/t5/stm32-mcus-wireless/cannot-write-tim-registers/m-p/791800/thread-id/24263#M24265

2 replies

Remi Demers
Associate II
April 2, 2025

I added LL_TIM_EnableDMAReq_UPDATE(TIM16); to the TIM16 configuration but it is still not working.

Remi Demers
Remi DemersAuthorBest answer
Associate II
April 9, 2025

This was caused by missing clock on the timer. See this case where it is solved.

https://community.st.com/t5/stm32-mcus-wireless/cannot-write-tim-registers/m-p/791800/thread-id/24263#M24265