Can't build TMAP_Central example: No rule to make target stm32wbaxx_ResetHandler_GCC.s
Hello,
I have a STM32WBA55G-DK1 board, and i'm trying to build the example code for the Unicast server (BLE_Audio_TMAP_Central example project).
I'm importing it using the GUI (new project, example, then i select the example).
I haven't modified anything in the code, but when i try to build it, i have the following error (see image bellow)

I tried to compile another example code (using the same steps as with the one giving errors), and it is working as intended.
Can you help me please? Thank you.
OS: Windows 11, last version
CubeIDE: last version