Associate II
July 15, 2025
Question
Can’t connect to target MCU on custom board based on STDES-WL5U4SBB (MB1720)
- July 15, 2025
- 1 reply
- 264 views
Hi ST Community,
I have developed a custom board based on the MB1720 HighBand HighPower A01 reference schematic (STM32WL series). On my custom board, I’m unable to debug the MCU — my debugger can’t connect to the target at all.
I’ve double-checked the power rails (VDDRF, VDDPA, VDDRF1V55) and they seem fine.
However, I’m not sure if I made any mistakes when replicating the debug interface or SMPS configuration.
Could you please help me check:
1.Is the debug circuit (SWD/JTAG lines, NRST, BOOT0) correctly implemented?
2.Are the power supply and SMPS sections connected properly for the STM32WL to boot and allow debugging?
3.Any common mistakes that could cause the debugger not to detect the target MCU?
I’ve attached my schematic