Clarification on LoRa FHSS vs LR-FHSS Support in STM32WLE5
Hi all,
I am currently working with the STM32WLE5JC for a LoRa/LoRaWAN-based IoT node and would like to clarify some points regarding LoRa FHSS and LR-FHSS support.
From several discussions in the STMicroelectronics Community, I noted the following statements from ST employees and contributors:
- “There is no way to activate the frequency hopping as the LoRa stack does not offer this feature on the STM32WL.”
- “After further investigation, it appears that the Semtech SX1262 does not support LoRa FHSS, (but supports for LR FHSS). This is a hardware limitation rather than a driver limitation.”
- “There is no reference to LoRa FHSS in the driver code or documentation.”
It is also understood that:
- Semtech SX1262 RF IP (which the STM32WLE5 is based on) does not support LoRa FHSS from a hardware perspective
Based on this, my understanding is that:
:backhand_index_pointing_right: STM32WLE5JC does not support LoRa FHSS
However, I would like clarification on the following:
1. LoRa FHSS Support
- Can you confirm definitively whether STM32WLE5JC has any level of support for LoRa FHSS?
- Is it strictly a hardware limitation (due to SX1262 architecture), or is there any possibility via firmware/stack-level implementation?
2. LR-FHSS Support
Since LR-FHSS is part of newer LoRaWAN specifications:
- Does STM32WLE5JC support LR-FHSS PHY mode (either fully or partially)?
- If yes, is this supported at:
- Hardware level
- Or via LoRaWAN stack (e.g., middleware updates)?
3. US915 Compatibility
If LoRa FHSS is not supported:
- Can STM32WLE5-based nodes still be fully compatible with LoRaWAN gateways operating in the US915 band?
- Since US915 involves channel hopping requirements, how is this handled without LoRa FHSS?
4. Future Support / Roadmap
Are there any:
- Planned enhancements or updates to enable support for LoRa-FHSS on STM32WLE5?
- Any potential support or enablement for LoRa FHSS, or is this permanently not supported due to hardware constraints?
- Any possible workarounds or alternative approaches to achieve compatibility where FHSS mechanisms are required?
My main goal is to ensure that a design based on STM32WLE5JC remains compliant and interoperable, especially in regions like US915 where hopping mechanisms are relevant.
Any clarification or guidance from ST experts or the community would be greatly appreciated.
Thank You