Question
Clarification on P-NUCLEO-LRWAN1 Obsolescence and Component Status
I noticed that the STM product P-NUCLEO-LRWAN1 is marked as obsolete. This kit includes the Nucleo-L073RZ and the SX1272MB2xAS LoRa® extension board. However, when searching for these components individually, both are still listed as active.
This situation raises a few questions:
- Does the obsolescence of the P-NUCLEO-LRWAN1 mean only the bundle is discontinued, while the individual components are still in production?
- Are there any official alternatives or updated bundles recommended for prototyping LoRa® solutions using STM32?
- If I purchase the Nucleo-L073RZ and SX1272MB2xAS separately, will the same software, documentation, and support as provided with the original kit still be available?
I’d appreciate any guidance or clarification from the community or those familiar with this kit.
Thank you!