Confusing STM32WB0 prices
Looking through the WB0x portfolio, it looks like the WB06 and WB07 VFQFPN are completely unattractive and even the WLCSP not a good bargain.
STM32WB06KC is supposed to be 1.87 Dollars, whereas STM32WB09KE stands at 1.013 Dollars.
Also the later would actually make a *** of the stm32U083KC as long as you don't need USB, since it is supposed to use less power, has double the Flash, more RAM (and BLE of course) and costs 25% less.
Actual listings at DigiKey and Mouser back up the budgetary claims. So what's up with those prices?
EDIT: Really, you censor the word F o o l ?