Custom bootloader doesn't jump to app
Hi all,
I'm trying to create a custom bootloader with openbl on rak3172 sip buil with stm32wl, so Ive used this repos here. I've just ipdate the main like this
#define APP_ADDRESS 0x08008000U
HAL_PWR_EnableBkUpAccess();
__HAL_RCC_RTC_ENABLE();
init_led();
if(get_bootloader_flag() == BOOTLOADER_MAGIC){
set_led_bootloader();
OpenBootloader_Init();
while (1)
{
OpenBootloader_ProtocolDetection();
}
}else{
set_led();
jump_to_app(APP_ADDRESS);
}
void jump_to_app(uint32_t address)
{
uint32_t i=0;
void (*SysMemBootJump)(void);
__disable_irq();
/* Disable Systick timer */
SysTick->CTRL = 0;
/* Set the clock to the default state */
HAL_RCC_DeInit();
/* Clear Interrupt Enable Register & Interrupt Pending Register */
for (i=0;i<5;i++)
{
NVIC->ICER[i]=0xFFFFFFFF;
NVIC->ICPR[i]=0xFFFFFFFF;
}
/* Re-enable all interrupts */
__enable_irq();
/* Set up the jump to boot loader address + 4 */
SysMemBootJump = (void (*)(void)) (*((uint32_t *) ((APP_ADDRESS + 4))));
/* Set the main stack pointer to the boot loader stack */
__set_MSP(*(uint32_t *)APP_ADDRESS);
/* Call the function to jump to boot loader location */
SysMemBootJump();
}
I check if I have a flag, if not jump to app. I flash bootloader with cube programmer, and after thaht I flash my app also with cube programmer at 0x08008000, to confirm I read flash with cube programmer and I'm able to see data at 0x08000000 and 0x08008000.
My linker script for my app
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 64K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x08008000, LENGTH = 256K - 0x8000
}
and system_stm32wlxx.c file
#define USER_VECT_TAB_ADDRESS
#define VECT_TAB_BASE_ADDRESS FLASH_BASE
#define VECT_TAB_OFFSET 0x00008000U
void SystemInit(void)
{
#if defined(USER_VECT_TAB_ADDRESS)
/* Configure the Vector Table location add offset address ------------------*/
SCB->VTOR = VECT_TAB_BASE_ADDRESS | VECT_TAB_OFFSET;
#endif
/* FPU settings ------------------------------------------------------------*/
#if (__FPU_PRESENT == 1) && (__FPU_USED == 1)
SCB->CPACR |= ((3UL << (10UL*2UL))|(3UL << (11UL*2UL))); /* set CP10 and CP11 Full Access */
#endif
}
I can see my led set in my case with set_led(), but my bootloader doesn't jump to my app. What I missed?
EDIT: ok so if I comment __enable_irq() in jump_to_app() I'm able to see the begining f my app with UART, but app stuck at first Hal_Delay... If I uncomment __enable_irq() my app never start... What happen ?