Skip to main content
Davide Dalfra
Associate III
May 7, 2025
Solved

Get Version bootloader command ignored on STM32WB09KE

  • May 7, 2025
  • 3 replies
  • 679 views

Hello,

 

I'm encountering the same issue, and i started debugging the embedded bootloader protocol manually. 
Or i'm starting getting crazy, but what specified in AN3155 is not respecting what i'm having on the serial port.
I'm using NUCLEO-WB09KE(MB2032B) mounted on MB1801D.

When moving JP1[MB2032B] to BOOT mode, SWD is not available.I'm only be able to get on bootloader mode (not with CubeProg) but as below.

Problem 1 - GetVersionComand (documentation mismatch)

I sucessfully entered in BL (Ack = 0x79), however GetVersion command is totally ignored. 
I then tested with another command to see if the communication with embedded BL works.
Something worked but not as expected.
DavideDalfra_0-1746622886252.png

 

DavideDalfra_1-1746623030630.png

Command 0x02+0xFD should reply with ACK(0x79) + N=NumberOfByte + PID. I did not see 0x79 as ACK nor the number of bytes i should get: i just got 0xD0 and 0x94.
I can't find what is the DEV_ID of STM32WB09KEx, so i can't verify if what'i'm having is really the DEV_ID or something else. Anyway the ACK is still missing.

What's happening there? I get into this because seems the SWD port is disabled due to low-power firmware pre-loaded on the board, so i tried to erase the firmware by accessing the rommed BL. As i was not able to get trough STM32PROG i decided to go "manual way".

Unfortunately after a mass erase i can't access anyway.
As i found mismatch command & replies referred to Uart BL specs, i have doubt i really erased the flash.

Anyone have some direction to point me out?


 

Thanks

Davide




Best answer by STTwo-32

Hello @Davide Dalfra 

I've tested using the STM32CubeProgrammer V2.19.0 and the NUCLEO-WB09KE. I've set the JP1 of the MB2032 to bootloader mode, connected the board throw the STM32CubeProgrammer, set the connection parameters as follow (with no parity):

STTwo32_0-1746720753339.png

Finally, click on connect and on the HW reset button of the board. Everything works fine for me:

 

16:30:03:448 : UR connection mode is defined with the HWrst reset mode
16:30:03:452 : RTS low
16:30:03:453 : DTR low
16:30:03:462 : Serial Port COM29 is successfully opened.
16:30:03:462 : Port configuration: parity = none, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
16:30:03:463 : No Init bits value is : 0 
16:30:03:463 : Sending init command: 
16:30:03:463 : #byte 0x7F sent successfully to target
16:30:07:463 : Wait ends after 2 loop, dataready = 0, delay = 4000
16:30:07:465 : Timeout error occured while waiting for acknowledgement.
16:30:07:465 : No response from target received
16:30:07:465 : Retrying UART init connection...
16:30:07:466 : #byte 0x7F sent successfully to target
16:30:07:468 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:468 : #ack Received response from target: 0x79
16:30:07:468 : Activating device: OK
16:30:07:469 : Board : --
16:30:07:469 : Sending GetID command and its XOR:
16:30:07:469 : #byte 0x02 sent successfully to target
16:30:07:469 : #byte 0xFD sent successfully to target
16:30:07:471 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:471 : #ack Received response from target: 0x79
16:30:07:472 : Received 4 data bytes from target : 0x03000106
16:30:07:472 : Chip ID: 0x32 
16:30:07:472 : Sending Get command and its XOR:
16:30:07:473 : #byte 0x00 sent successfully to target
16:30:07:473 : #byte 0xFF sent successfully to target
16:30:07:473 : #ack Received response from target: 0x79
16:30:07:475 : Received 3 data bytes from target : 0x790901
16:30:07:475 : size of bytes in the response: 9
16:30:07:476 : Received 9 data bytes from target
16:30:07:477 : Full received response: 790901000102112131438292
16:30:07:477 : BootLoader protocol version: 1.0
16:30:07:477 : #byte 0x11 sent successfully to target
16:30:07:478 : #byte 0xEE sent successfully to target
16:30:07:570 : #data sent successfully to target: 0x1004000014
16:30:07:570 : #byte 0x00 sent successfully to target
16:30:07:571 : #byte 0xFF sent successfully to target
16:30:07:573 : Sending GetID command and its XOR:
16:30:07:573 : #byte 0x02 sent successfully to target
16:30:07:573 : #byte 0xFD sent successfully to target
16:30:07:573 : #ack Received response from target: 0x00
16:30:07:575 : Received 5 data bytes from target : 0x7903000106
16:30:07:579 : #byte 0x11 sent successfully to target
16:30:07:580 : #byte 0xEE sent successfully to target
16:30:07:679 : #data sent successfully to target: 0x1004000014
16:30:07:679 : #byte 0x00 sent successfully to target
16:30:07:682 : #byte 0xFF sent successfully to target
16:30:07:685 : Sending GetID command and its XOR:
16:30:07:685 : #byte 0x02 sent successfully to target
16:30:07:685 : #byte 0xFD sent successfully to target
16:30:07:685 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:685 : #ack Received response from target: 0x79
16:30:07:687 : Received 5 data bytes from target : 0x030001061f
16:30:09:894 : Sending GetID command and its XOR:
16:30:09:894 : #byte 0x02 sent successfully to target
16:30:09:894 : bytesToWrite before send = 1 
16:30:09:894 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:09:894 : waitForBytesWritten Error : The wait operation timed out.
16:30:09:894 : #byte 0xFD sent successfully to target
16:30:09:895 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:895 : #ack Received response from target: 0x79
16:30:09:895 : Received 5 data bytes from target : 0x030001061f
16:30:09:895 : UPLOADING OPTION BYTES DATA ...
16:30:09:896 : Bank : 0x00
16:30:09:896 : Address : 0x10040000
16:30:09:896 : Size : 16 Bytes
16:30:09:896 : Sending Read command and its XOR:
16:30:09:896 : #byte 0x11 sent successfully to target
16:30:09:897 : #byte 0xEE sent successfully to target
16:30:09:897 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:897 : #ack Received response from target: 0x79
16:30:09:899 : Sending Read address and its checksum:
16:30:09:899 : #data sent successfully to target: 0x1004000014
16:30:09:899 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:899 : #ack Received response from target: 0x79
16:30:09:900 : Sending number of bytes to be read - 1 and its checksum:
16:30:09:900 : #data sent successfully to target: 0x0ff0
16:30:09:900 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:900 : #ack Received response from target: 0x79
16:30:09:900 : Received 16 data bytes from target
16:30:09:902 : UPLOADING OPTION BYTES DATA ...
16:30:09:902 : Bank : 0x00
16:30:09:902 : Address : 0x10040000
16:30:09:902 : Size : 16 Bytes
16:30:09:902 : Sending Read command and its XOR:
16:30:09:902 : #byte 0x11 sent successfully to target
16:30:09:903 : #byte 0xEE sent successfully to target
16:30:09:903 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:903 : #ack Received response from target: 0x79
16:30:09:903 : Sending Read address and its checksum:
16:30:09:903 : #data sent successfully to target: 0x1004000014
16:30:09:903 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:903 : #ack Received response from target: 0x79
16:30:09:903 : Sending number of bytes to be read - 1 and its checksum:
16:30:09:903 : #data sent successfully to target: 0x0ff0
16:30:09:904 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:904 : #ack Received response from target: 0x79
16:30:09:904 : Received 16 data bytes from target
16:30:09:904 : Sending GetID command and its XOR:
16:30:09:904 : #byte 0x02 sent successfully to target
16:30:09:904 : bytesToWrite before send = 1 
16:30:09:904 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:09:904 : waitForBytesWritten Error : The wait operation timed out.
16:30:09:905 : #byte 0xFD sent successfully to target
16:30:09:905 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:905 : #ack Received response from target: 0x79
16:30:09:905 : Received 5 data bytes from target : 0x030001061f
16:30:09:905 : Sending GetID command and its XOR:
16:30:09:906 : #byte 0x02 sent successfully to target
16:30:09:906 : #byte 0xFD sent successfully to target
16:30:09:906 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:906 : #ack Received response from target: 0x79
16:30:09:907 : Received 5 data bytes from target : 0x030001061f
16:30:09:907 : UPLOADING ...
16:30:09:907 : Size : 1024 Bytes
16:30:09:907 : Address : 0x10040000
16:30:09:907 : Read progress:
16:30:09:908 : Sending Read command and its XOR:
16:30:09:908 : #byte 0x11 sent successfully to target
16:30:09:908 : bytesToWrite before send = 1 
16:30:09:909 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:10:853 : waitForBytesWritten Error : The wait operation timed out.
16:30:10:874 : #byte 0xEE sent successfully to target
16:30:10:874 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:874 : #ack Received response from target: 0x79
16:30:10:881 : Sending Read address and its checksum:
16:30:10:881 : #data sent successfully to target: 0x1004000014
16:30:10:884 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:884 : #ack Received response from target: 0x79
16:30:10:885 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:885 : #data sent successfully to target: 0xff00
16:30:10:885 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:885 : #ack Received response from target: 0x79
16:30:10:906 : Received 256 data bytes from target
16:30:10:906 : Sending Read command and its XOR:
16:30:10:906 : #byte 0x11 sent successfully to target
16:30:10:906 : #byte 0xEE sent successfully to target
16:30:10:906 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:907 : #ack Received response from target: 0x79
16:30:10:907 : Sending Read address and its checksum:
16:30:10:907 : #data sent successfully to target: 0x1004010015
16:30:10:907 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:907 : #ack Received response from target: 0x79
16:30:10:907 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:907 : #data sent successfully to target: 0xff00
16:30:10:909 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:910 : #ack Received response from target: 0x79
16:30:10:940 : Received 256 data bytes from target
16:30:10:940 : Sending Read command and its XOR:
16:30:10:941 : #byte 0x11 sent successfully to target
16:30:10:941 : #byte 0xEE sent successfully to target
16:30:10:941 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:941 : #ack Received response from target: 0x79
16:30:10:941 : Sending Read address and its checksum:
16:30:10:941 : #data sent successfully to target: 0x1004020016
16:30:10:941 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:941 : #ack Received response from target: 0x79
16:30:10:941 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:942 : #data sent successfully to target: 0xff00
16:30:10:942 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:942 : #ack Received response from target: 0x79
16:30:10:986 : Received 256 data bytes from target
16:30:10:987 : Sending Read command and its XOR:
16:30:10:987 : #byte 0x11 sent successfully to target
16:30:10:987 : #byte 0xEE sent successfully to target
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:987 : #ack Received response from target: 0x79
16:30:10:987 : Sending Read address and its checksum:
16:30:10:987 : #data sent successfully to target: 0x1004030017
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:987 : #ack Received response from target: 0x79
16:30:10:987 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:987 : #data sent successfully to target: 0xff00
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:988 : #ack Received response from target: 0x79
16:30:10:988 : Received 256 data bytes from target
16:30:10:988 : Data read successfully
16:30:10:988 : Time elapsed during the read operation is: 00:00:01.136
16:30:12:007 : Sending GetID command and its XOR:
16:30:12:008 : #byte 0x02 sent successfully to target
16:30:12:008 : bytesToWrite before send = 1 
16:30:12:008 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:12:095 : waitForBytesWritten Error : The wait operation timed out.
16:30:12:095 : #byte 0xFD sent successfully to target
16:30:12:096 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:12:096 : #ack Received response from target: 0x79
16:30:12:096 : Received 5 data bytes from target : 0x030001061f
16:30:12:096 : Sending GetID command and its XOR:
16:30:12:096 : #byte 0x02 sent successfully to target
16:30:12:096 : #byte 0xFD sent successfully to target
16:30:12:096 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:12:096 : #ack Received response from target: 0x79
16:30:12:097 : Received 5 data bytes from target : 0x030001061f
16:30:13:008 : Sending GetID command and its XOR:
16:30:13:008 : #byte 0x02 sent successfully to target
16:30:13:014 : #byte 0xFD sent successfully to target
16:30:13:014 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:13:014 : #ack Received response from target: 0x79
16:30:13:014 : Received 5 data bytes from target : 0x030001061f
16:30:13:015 : Sending GetID command and its XOR:
16:30:13:015 : #byte 0x02 sent successfully to target
16:30:13:015 : #byte 0xFD sent successfully to target
16:30:13:015 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:13:016 : #ack Received response from target: 0x79
16:30:13:016 : Received 5 data bytes from target : 0x030001061f
16:30:14:014 : Sending GetID command and its XOR:
16:30:14:015 : #byte 0x02 sent successfully to target
16:30:14:021 : #byte 0xFD sent successfully to target
16:30:14:021 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:14:022 : #ack Received response from target: 0x79
16:30:14:024 : Received 5 data bytes from target : 0x030001061f
16:30:14:024 : Sending GetID command and its XOR:
16:30:14:024 : #byte 0x02 sent successfully to target
16:30:14:024 : #byte 0xFD sent successfully to target
16:30:14:024 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:14:025 : #ack Received response from target: 0x79
16:30:14:025 : Received 5 data bytes from target : 0x030001061f
16:30:15:020 : Sending GetID command and its XOR:
16:30:15:020 : #byte 0x02 sent successfully to target
16:30:15:025 : #byte 0xFD sent successfully to target
16:30:15:029 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:15:029 : #ack Received response from target: 0x79
16:30:15:030 : Received 5 data bytes from target : 0x030001061f
16:30:15:030 : Sending GetID command and its XOR:
16:30:15:030 : #byte 0x02 sent successfully to target
16:30:15:030 : #byte 0xFD sent successfully to target
16:30:15:030 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:15:030 : #ack Received response from target: 0x79
16:30:15:033 : Received 5 data bytes from target : 0x030001061f
16:30:16:026 : Sending GetID command and its XOR:
16:30:16:027 : #byte 0x02 sent successfully to target
16:30:16:036 : #byte 0xFD sent successfully to target
16:30:16:037 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:16:037 : #ack Received response from target: 0x79
16:30:16:039 : Received 5 data bytes from target : 0x030001061f
16:30:16:040 : Sending GetID command and its XOR:
16:30:16:040 : #byte 0x02 sent successfully to target
16:30:16:040 : #byte 0xFD sent successfully to target
16:30:16:040 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:16:040 : #ack Received response from target: 0x79
16:30:16:041 : Received 5 data bytes from target : 0x030001061f
16:30:17:033 : Sending GetID command and its XOR:
16:30:17:033 : #byte 0x02 sent successfully to target
16:30:17:036 : #byte 0xFD sent successfully to target
16:30:17:038 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:17:038 : #ack Received response from target: 0x79
16:30:17:040 : Received 5 data bytes from target : 0x030001061f
16:30:17:040 : Sending GetID command and its XOR:
16:30:17:040 : #byte 0x02 sent successfully to target
16:30:17:041 : #byte 0xFD sent successfully to target
16:30:17:044 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:17:044 : #ack Received response from target: 0x79
16:30:17:050 : Received 5 data bytes from target : 0x030001061f
16:30:18:039 : Sending GetID command and its XOR:
16:30:18:040 : #byte 0x02 sent successfully to target
16:30:18:043 : #byte 0xFD sent successfully to target
16:30:18:046 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:18:047 : #ack Received response from target: 0x79
16:30:18:047 : Received 5 data bytes from target : 0x030001061f
16:30:18:047 : Sending GetID command and its XOR:
16:30:18:047 : #byte 0x02 sent successfully to target
16:30:18:047 : #byte 0xFD sent successfully to target
16:30:18:048 : #ack Received response from target: 0x79
16:30:18:051 : Received 5 data bytes from target : 0x7903000106
16:30:19:045 : Sending GetID command and its XOR:
16:30:19:045 : #byte 0x02 sent successfully to target
16:30:19:051 : #byte 0xFD sent successfully to target
16:30:19:054 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:19:054 : #ack Received response from target: 0x79
16:30:19:054 : Received 5 data bytes from target : 0x030001061f
16:30:19:054 : Sending GetID command and its XOR:
16:30:19:054 : #byte 0x02 sent successfully to target
16:30:19:055 : #byte 0xFD sent successfully to target
16:30:19:055 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:19:055 : #ack Received response from target: 0x79
16:30:19:056 : Received 5 data bytes from target : 0x030001061f
16:30:20:051 : Sending GetID command and its XOR:
16:30:20:052 : #byte 0x02 sent successfully to target
16:30:20:058 : #byte 0xFD sent successfully to target
16:30:20:062 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:20:062 : #ack Received response from target: 0x79
16:30:20:062 : Received 5 data bytes from target : 0x030001061f
16:30:20:062 : Sending GetID command and its XOR:
16:30:20:062 : #byte 0x02 sent successfully to target
16:30:20:062 : #byte 0xFD sent successfully to target
16:30:20:062 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:20:063 : #ack Received response from target: 0x79
16:30:20:063 : Received 5 data bytes from target : 0x030001061f
16:30:21:059 : Sending GetID command and its XOR:
16:30:21:059 : #byte 0x02 sent successfully to target
16:30:21:062 : #byte 0xFD sent successfully to target
16:30:21:067 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:21:067 : #ack Received response from target: 0x79
16:30:21:067 : Received 5 data bytes from target : 0x030001061f
16:30:21:067 : Sending GetID command and its XOR:
16:30:21:067 : #byte 0x02 sent successfully to target
16:30:21:068 : #byte 0xFD sent successfully to target
16:30:21:070 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:21:070 : #ack Received response from target: 0x79
16:30:21:070 : Received 5 data bytes from target : 0x030001061f
16:30:22:065 : Sending GetID command and its XOR:
16:30:22:066 : #byte 0x02 sent successfully to target
16:30:22:071 : #byte 0xFD sent successfully to target
16:30:22:075 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:22:076 : #ack Received response from target: 0x79
16:30:22:076 : Received 5 data bytes from target : 0x030001061f
16:30:22:076 : Sending GetID command and its XOR:
16:30:22:076 : #byte 0x02 sent successfully to target
16:30:22:076 : #byte 0xFD sent successfully to target
16:30:22:077 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:22:077 : #ack Received response from target: 0x79
16:30:22:077 : Received 5 data bytes from target : 0x030001061f
16:30:23:073 : Sending GetID command and its XOR:
16:30:23:073 : #byte 0x02 sent successfully to target
16:30:23:073 : #byte 0xFD sent successfully to target
16:30:23:073 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:23:073 : #ack Received response from target: 0x79
16:30:23:089 : Received 5 data bytes from target : 0x030001061f
16:30:23:090 : Sending GetID command and its XOR:
16:30:23:090 : #byte 0x02 sent successfully to target
16:30:23:090 : #byte 0xFD sent successfully to target
16:30:23:090 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:23:090 : #ack Received response from target: 0x79
16:30:23:090 : Received 5 data bytes from target : 0x030001061f
16:30:24:079 : Sending GetID command and its XOR:
16:30:24:080 : #byte 0x02 sent successfully to target
16:30:24:080 : #byte 0xFD sent successfully to target
16:30:24:085 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:24:085 : #ack Received response from target: 0x79
16:30:24:091 : Received 5 data bytes from target : 0x030001061f
16:30:24:091 : Sending GetID command and its XOR:
16:30:24:092 : #byte 0x02 sent successfully to target
16:30:24:092 : #byte 0xFD sent successfully to target
16:30:24:092 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:24:092 : #ack Received response from target: 0x79
16:30:24:092 : Received 5 data bytes from target : 0x030001061f
16:30:24:671 : UART PORT CLOSE 
16:30:24:684 : Disconnected from device.

I think the problem on your side is to use the even parity.

Best Regards.

STTwo-32

3 replies

TDK
Super User
May 7, 2025

Even parity?

STM32CubeProgrammer can access the bootloader over UART, I'd try that.

TDK_0-1746630341766.png

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
Davide Dalfra
Associate III
May 8, 2025

Yes even parity and with STM32CubeProgrammer first.
I go "manual" because i was getting peanuts from Cube so i wanted to understand.

By enablihng Verbosity level 3 on STM32CubeProgrammer i'm getting the same results (ack missing).

DavideDalfra_0-1746684011712.png

07:59:37:428 : UR connection mode is defined with the HWrst reset mode
 07:59:37:431 : RTS low
 07:59:37:431 : DTR low
 07:59:37:438 : Serial Port COM3 is successfully opened.
 07:59:37:438 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
 07:59:37:438 : No Init bits value is : 0 
 07:59:37:438 : Sending init command: 
 07:59:37:438 : byte 0x7F sent successfully to target
 07:59:37:439 : Wait ends after 1 loop, dataready = 1, delay = 0
 07:59:37:439 : Received response from target: 0x79
 07:59:37:448 : Activating device: OK
 07:59:37:448 : Board : --
 07:59:37:448 : Sending GetID command and its XOR:
 07:59:37:449 : byte 0x02 sent successfully to target
 07:59:37:449 : byte 0xFD sent successfully to target
 07:59:37:452 : Wait ends after 1 loop, dataready = 1, delay = 0
 07:59:37:452 : Received response from target: 0xd0
 07:59:37:452 : Error: GETID command not acknowledged!
 07:59:37:552 : Reemission of GetID command
 07:59:37:552 : Sending GetID command and its XOR:
 07:59:37:553 : byte 0x02 sent successfully to target
 07:59:37:553 : byte 0xFD sent successfully to target
 07:59:37:553 : Received response from target: 0x94
 07:59:37:553 : Error: GETID command not acknowledged!
 07:59:37:652 : Reemission of GetID command
 07:59:37:652 : Sending GetID command and its XOR:
 07:59:37:652 : byte 0x02 sent successfully to target
 07:59:37:652 : byte 0xFD sent successfully to target
 07:59:37:653 : Received response from target: 0xd0
 07:59:37:653 : Error: GETID command not acknowledged!
 07:59:37:838 : Chip ID: 0x0 
 07:59:37:839 : UART PORT CLOSE 
 07:59:37:840 : Disconnected from device.
 07:59:37:840 : RTS low
 07:59:37:840 : DTR low
 07:59:37:845 : Serial Port COM3 is successfully opened.
 07:59:37:845 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
 07:59:37:845 : No Init bits value is : 0 
 07:59:37:845 : Sending init command: 
 07:59:37:846 : byte 0x7F sent successfully to target
 07:59:41:845 : Wait ends after 2 loop, dataready = 0, delay = 4000
 07:59:41:845 : Timeout error occured while waiting for acknowledgement.
 07:59:41:845 : No response from target received
 07:59:41:845 : Retrying UART init connection...
 07:59:41:846 : byte 0x7F sent successfully to target
 07:59:41:847 : Wait ends after 1 loop, dataready = 1, delay = 0
 07:59:41:847 : Received response from target: 0x1f
 07:59:41:847 : Activating device: OK
 07:59:41:847 : Board : --
 07:59:41:847 : Sending GetID command and its XOR:
 07:59:41:847 : byte 0x02 sent successfully to target
 07:59:41:848 : byte 0xFD sent successfully to target
 07:59:41:848 : Wait ends after 1 loop, dataready = 1, delay = 0
 07:59:41:848 : Received response from target: 0xd0
 07:59:41:848 : Error: GETID command not acknowledged!
 07:59:41:955 : Reemission of GetID command
 07:59:41:955 : Sending GetID command and its XOR:
 07:59:41:955 : byte 0x02 sent successfully to target
 07:59:41:956 : byte 0xFD sent successfully to target
 07:59:41:956 : Wait ends after 1 loop, dataready = 1, delay = 0
 07:59:41:956 : Received response from target: 0xd0
 07:59:41:956 : Error: GETID command not acknowledged!
 07:59:42:055 : Reemission of GetID command
 07:59:42:055 : Sending GetID command and its XOR:
 07:59:42:057 : byte 0x02 sent successfully to target
 07:59:42:057 : byte 0xFD sent successfully to target
 07:59:42:057 : Wait ends after 1 loop, dataready = 1, delay = 0
 07:59:42:057 : Received response from target: 0xd0
 07:59:42:057 : Error: GETID command not acknowledged!
 07:59:42:156 : Chip ID: 0x0 
 07:59:42:157 : UART PORT CLOSE 

 

Regards

Davide

 

 

 

TDK
Super User
May 8, 2025

Since this error is different from the post you originally replied to, I've moved it here. I've asked someone to take a look.

"If you feel a post has answered your question, please click ""Accept as Solution""."
STTwo-32
STTwo-32Best answer
Technical Moderator
May 8, 2025

Hello @Davide Dalfra 

I've tested using the STM32CubeProgrammer V2.19.0 and the NUCLEO-WB09KE. I've set the JP1 of the MB2032 to bootloader mode, connected the board throw the STM32CubeProgrammer, set the connection parameters as follow (with no parity):

STTwo32_0-1746720753339.png

Finally, click on connect and on the HW reset button of the board. Everything works fine for me:

 

16:30:03:448 : UR connection mode is defined with the HWrst reset mode
16:30:03:452 : RTS low
16:30:03:453 : DTR low
16:30:03:462 : Serial Port COM29 is successfully opened.
16:30:03:462 : Port configuration: parity = none, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
16:30:03:463 : No Init bits value is : 0 
16:30:03:463 : Sending init command: 
16:30:03:463 : #byte 0x7F sent successfully to target
16:30:07:463 : Wait ends after 2 loop, dataready = 0, delay = 4000
16:30:07:465 : Timeout error occured while waiting for acknowledgement.
16:30:07:465 : No response from target received
16:30:07:465 : Retrying UART init connection...
16:30:07:466 : #byte 0x7F sent successfully to target
16:30:07:468 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:468 : #ack Received response from target: 0x79
16:30:07:468 : Activating device: OK
16:30:07:469 : Board : --
16:30:07:469 : Sending GetID command and its XOR:
16:30:07:469 : #byte 0x02 sent successfully to target
16:30:07:469 : #byte 0xFD sent successfully to target
16:30:07:471 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:471 : #ack Received response from target: 0x79
16:30:07:472 : Received 4 data bytes from target : 0x03000106
16:30:07:472 : Chip ID: 0x32 
16:30:07:472 : Sending Get command and its XOR:
16:30:07:473 : #byte 0x00 sent successfully to target
16:30:07:473 : #byte 0xFF sent successfully to target
16:30:07:473 : #ack Received response from target: 0x79
16:30:07:475 : Received 3 data bytes from target : 0x790901
16:30:07:475 : size of bytes in the response: 9
16:30:07:476 : Received 9 data bytes from target
16:30:07:477 : Full received response: 790901000102112131438292
16:30:07:477 : BootLoader protocol version: 1.0
16:30:07:477 : #byte 0x11 sent successfully to target
16:30:07:478 : #byte 0xEE sent successfully to target
16:30:07:570 : #data sent successfully to target: 0x1004000014
16:30:07:570 : #byte 0x00 sent successfully to target
16:30:07:571 : #byte 0xFF sent successfully to target
16:30:07:573 : Sending GetID command and its XOR:
16:30:07:573 : #byte 0x02 sent successfully to target
16:30:07:573 : #byte 0xFD sent successfully to target
16:30:07:573 : #ack Received response from target: 0x00
16:30:07:575 : Received 5 data bytes from target : 0x7903000106
16:30:07:579 : #byte 0x11 sent successfully to target
16:30:07:580 : #byte 0xEE sent successfully to target
16:30:07:679 : #data sent successfully to target: 0x1004000014
16:30:07:679 : #byte 0x00 sent successfully to target
16:30:07:682 : #byte 0xFF sent successfully to target
16:30:07:685 : Sending GetID command and its XOR:
16:30:07:685 : #byte 0x02 sent successfully to target
16:30:07:685 : #byte 0xFD sent successfully to target
16:30:07:685 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:07:685 : #ack Received response from target: 0x79
16:30:07:687 : Received 5 data bytes from target : 0x030001061f
16:30:09:894 : Sending GetID command and its XOR:
16:30:09:894 : #byte 0x02 sent successfully to target
16:30:09:894 : bytesToWrite before send = 1 
16:30:09:894 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:09:894 : waitForBytesWritten Error : The wait operation timed out.
16:30:09:894 : #byte 0xFD sent successfully to target
16:30:09:895 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:895 : #ack Received response from target: 0x79
16:30:09:895 : Received 5 data bytes from target : 0x030001061f
16:30:09:895 : UPLOADING OPTION BYTES DATA ...
16:30:09:896 : Bank : 0x00
16:30:09:896 : Address : 0x10040000
16:30:09:896 : Size : 16 Bytes
16:30:09:896 : Sending Read command and its XOR:
16:30:09:896 : #byte 0x11 sent successfully to target
16:30:09:897 : #byte 0xEE sent successfully to target
16:30:09:897 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:897 : #ack Received response from target: 0x79
16:30:09:899 : Sending Read address and its checksum:
16:30:09:899 : #data sent successfully to target: 0x1004000014
16:30:09:899 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:899 : #ack Received response from target: 0x79
16:30:09:900 : Sending number of bytes to be read - 1 and its checksum:
16:30:09:900 : #data sent successfully to target: 0x0ff0
16:30:09:900 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:900 : #ack Received response from target: 0x79
16:30:09:900 : Received 16 data bytes from target
16:30:09:902 : UPLOADING OPTION BYTES DATA ...
16:30:09:902 : Bank : 0x00
16:30:09:902 : Address : 0x10040000
16:30:09:902 : Size : 16 Bytes
16:30:09:902 : Sending Read command and its XOR:
16:30:09:902 : #byte 0x11 sent successfully to target
16:30:09:903 : #byte 0xEE sent successfully to target
16:30:09:903 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:903 : #ack Received response from target: 0x79
16:30:09:903 : Sending Read address and its checksum:
16:30:09:903 : #data sent successfully to target: 0x1004000014
16:30:09:903 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:903 : #ack Received response from target: 0x79
16:30:09:903 : Sending number of bytes to be read - 1 and its checksum:
16:30:09:903 : #data sent successfully to target: 0x0ff0
16:30:09:904 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:904 : #ack Received response from target: 0x79
16:30:09:904 : Received 16 data bytes from target
16:30:09:904 : Sending GetID command and its XOR:
16:30:09:904 : #byte 0x02 sent successfully to target
16:30:09:904 : bytesToWrite before send = 1 
16:30:09:904 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:09:904 : waitForBytesWritten Error : The wait operation timed out.
16:30:09:905 : #byte 0xFD sent successfully to target
16:30:09:905 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:905 : #ack Received response from target: 0x79
16:30:09:905 : Received 5 data bytes from target : 0x030001061f
16:30:09:905 : Sending GetID command and its XOR:
16:30:09:906 : #byte 0x02 sent successfully to target
16:30:09:906 : #byte 0xFD sent successfully to target
16:30:09:906 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:09:906 : #ack Received response from target: 0x79
16:30:09:907 : Received 5 data bytes from target : 0x030001061f
16:30:09:907 : UPLOADING ...
16:30:09:907 : Size : 1024 Bytes
16:30:09:907 : Address : 0x10040000
16:30:09:907 : Read progress:
16:30:09:908 : Sending Read command and its XOR:
16:30:09:908 : #byte 0x11 sent successfully to target
16:30:09:908 : bytesToWrite before send = 1 
16:30:09:909 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:10:853 : waitForBytesWritten Error : The wait operation timed out.
16:30:10:874 : #byte 0xEE sent successfully to target
16:30:10:874 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:874 : #ack Received response from target: 0x79
16:30:10:881 : Sending Read address and its checksum:
16:30:10:881 : #data sent successfully to target: 0x1004000014
16:30:10:884 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:884 : #ack Received response from target: 0x79
16:30:10:885 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:885 : #data sent successfully to target: 0xff00
16:30:10:885 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:885 : #ack Received response from target: 0x79
16:30:10:906 : Received 256 data bytes from target
16:30:10:906 : Sending Read command and its XOR:
16:30:10:906 : #byte 0x11 sent successfully to target
16:30:10:906 : #byte 0xEE sent successfully to target
16:30:10:906 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:907 : #ack Received response from target: 0x79
16:30:10:907 : Sending Read address and its checksum:
16:30:10:907 : #data sent successfully to target: 0x1004010015
16:30:10:907 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:907 : #ack Received response from target: 0x79
16:30:10:907 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:907 : #data sent successfully to target: 0xff00
16:30:10:909 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:910 : #ack Received response from target: 0x79
16:30:10:940 : Received 256 data bytes from target
16:30:10:940 : Sending Read command and its XOR:
16:30:10:941 : #byte 0x11 sent successfully to target
16:30:10:941 : #byte 0xEE sent successfully to target
16:30:10:941 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:941 : #ack Received response from target: 0x79
16:30:10:941 : Sending Read address and its checksum:
16:30:10:941 : #data sent successfully to target: 0x1004020016
16:30:10:941 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:941 : #ack Received response from target: 0x79
16:30:10:941 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:942 : #data sent successfully to target: 0xff00
16:30:10:942 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:942 : #ack Received response from target: 0x79
16:30:10:986 : Received 256 data bytes from target
16:30:10:987 : Sending Read command and its XOR:
16:30:10:987 : #byte 0x11 sent successfully to target
16:30:10:987 : #byte 0xEE sent successfully to target
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:987 : #ack Received response from target: 0x79
16:30:10:987 : Sending Read address and its checksum:
16:30:10:987 : #data sent successfully to target: 0x1004030017
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:987 : #ack Received response from target: 0x79
16:30:10:987 : Sending number of bytes to be read - 1 and its checksum:
16:30:10:987 : #data sent successfully to target: 0xff00
16:30:10:987 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:10:988 : #ack Received response from target: 0x79
16:30:10:988 : Received 256 data bytes from target
16:30:10:988 : Data read successfully
16:30:10:988 : Time elapsed during the read operation is: 00:00:01.136
16:30:12:007 : Sending GetID command and its XOR:
16:30:12:008 : #byte 0x02 sent successfully to target
16:30:12:008 : bytesToWrite before send = 1 
16:30:12:008 : bFlushRet = 1, bytesToWrite after flush() = 1 
16:30:12:095 : waitForBytesWritten Error : The wait operation timed out.
16:30:12:095 : #byte 0xFD sent successfully to target
16:30:12:096 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:12:096 : #ack Received response from target: 0x79
16:30:12:096 : Received 5 data bytes from target : 0x030001061f
16:30:12:096 : Sending GetID command and its XOR:
16:30:12:096 : #byte 0x02 sent successfully to target
16:30:12:096 : #byte 0xFD sent successfully to target
16:30:12:096 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:12:096 : #ack Received response from target: 0x79
16:30:12:097 : Received 5 data bytes from target : 0x030001061f
16:30:13:008 : Sending GetID command and its XOR:
16:30:13:008 : #byte 0x02 sent successfully to target
16:30:13:014 : #byte 0xFD sent successfully to target
16:30:13:014 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:13:014 : #ack Received response from target: 0x79
16:30:13:014 : Received 5 data bytes from target : 0x030001061f
16:30:13:015 : Sending GetID command and its XOR:
16:30:13:015 : #byte 0x02 sent successfully to target
16:30:13:015 : #byte 0xFD sent successfully to target
16:30:13:015 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:13:016 : #ack Received response from target: 0x79
16:30:13:016 : Received 5 data bytes from target : 0x030001061f
16:30:14:014 : Sending GetID command and its XOR:
16:30:14:015 : #byte 0x02 sent successfully to target
16:30:14:021 : #byte 0xFD sent successfully to target
16:30:14:021 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:14:022 : #ack Received response from target: 0x79
16:30:14:024 : Received 5 data bytes from target : 0x030001061f
16:30:14:024 : Sending GetID command and its XOR:
16:30:14:024 : #byte 0x02 sent successfully to target
16:30:14:024 : #byte 0xFD sent successfully to target
16:30:14:024 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:14:025 : #ack Received response from target: 0x79
16:30:14:025 : Received 5 data bytes from target : 0x030001061f
16:30:15:020 : Sending GetID command and its XOR:
16:30:15:020 : #byte 0x02 sent successfully to target
16:30:15:025 : #byte 0xFD sent successfully to target
16:30:15:029 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:15:029 : #ack Received response from target: 0x79
16:30:15:030 : Received 5 data bytes from target : 0x030001061f
16:30:15:030 : Sending GetID command and its XOR:
16:30:15:030 : #byte 0x02 sent successfully to target
16:30:15:030 : #byte 0xFD sent successfully to target
16:30:15:030 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:15:030 : #ack Received response from target: 0x79
16:30:15:033 : Received 5 data bytes from target : 0x030001061f
16:30:16:026 : Sending GetID command and its XOR:
16:30:16:027 : #byte 0x02 sent successfully to target
16:30:16:036 : #byte 0xFD sent successfully to target
16:30:16:037 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:16:037 : #ack Received response from target: 0x79
16:30:16:039 : Received 5 data bytes from target : 0x030001061f
16:30:16:040 : Sending GetID command and its XOR:
16:30:16:040 : #byte 0x02 sent successfully to target
16:30:16:040 : #byte 0xFD sent successfully to target
16:30:16:040 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:16:040 : #ack Received response from target: 0x79
16:30:16:041 : Received 5 data bytes from target : 0x030001061f
16:30:17:033 : Sending GetID command and its XOR:
16:30:17:033 : #byte 0x02 sent successfully to target
16:30:17:036 : #byte 0xFD sent successfully to target
16:30:17:038 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:17:038 : #ack Received response from target: 0x79
16:30:17:040 : Received 5 data bytes from target : 0x030001061f
16:30:17:040 : Sending GetID command and its XOR:
16:30:17:040 : #byte 0x02 sent successfully to target
16:30:17:041 : #byte 0xFD sent successfully to target
16:30:17:044 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:17:044 : #ack Received response from target: 0x79
16:30:17:050 : Received 5 data bytes from target : 0x030001061f
16:30:18:039 : Sending GetID command and its XOR:
16:30:18:040 : #byte 0x02 sent successfully to target
16:30:18:043 : #byte 0xFD sent successfully to target
16:30:18:046 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:18:047 : #ack Received response from target: 0x79
16:30:18:047 : Received 5 data bytes from target : 0x030001061f
16:30:18:047 : Sending GetID command and its XOR:
16:30:18:047 : #byte 0x02 sent successfully to target
16:30:18:047 : #byte 0xFD sent successfully to target
16:30:18:048 : #ack Received response from target: 0x79
16:30:18:051 : Received 5 data bytes from target : 0x7903000106
16:30:19:045 : Sending GetID command and its XOR:
16:30:19:045 : #byte 0x02 sent successfully to target
16:30:19:051 : #byte 0xFD sent successfully to target
16:30:19:054 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:19:054 : #ack Received response from target: 0x79
16:30:19:054 : Received 5 data bytes from target : 0x030001061f
16:30:19:054 : Sending GetID command and its XOR:
16:30:19:054 : #byte 0x02 sent successfully to target
16:30:19:055 : #byte 0xFD sent successfully to target
16:30:19:055 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:19:055 : #ack Received response from target: 0x79
16:30:19:056 : Received 5 data bytes from target : 0x030001061f
16:30:20:051 : Sending GetID command and its XOR:
16:30:20:052 : #byte 0x02 sent successfully to target
16:30:20:058 : #byte 0xFD sent successfully to target
16:30:20:062 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:20:062 : #ack Received response from target: 0x79
16:30:20:062 : Received 5 data bytes from target : 0x030001061f
16:30:20:062 : Sending GetID command and its XOR:
16:30:20:062 : #byte 0x02 sent successfully to target
16:30:20:062 : #byte 0xFD sent successfully to target
16:30:20:062 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:20:063 : #ack Received response from target: 0x79
16:30:20:063 : Received 5 data bytes from target : 0x030001061f
16:30:21:059 : Sending GetID command and its XOR:
16:30:21:059 : #byte 0x02 sent successfully to target
16:30:21:062 : #byte 0xFD sent successfully to target
16:30:21:067 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:21:067 : #ack Received response from target: 0x79
16:30:21:067 : Received 5 data bytes from target : 0x030001061f
16:30:21:067 : Sending GetID command and its XOR:
16:30:21:067 : #byte 0x02 sent successfully to target
16:30:21:068 : #byte 0xFD sent successfully to target
16:30:21:070 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:21:070 : #ack Received response from target: 0x79
16:30:21:070 : Received 5 data bytes from target : 0x030001061f
16:30:22:065 : Sending GetID command and its XOR:
16:30:22:066 : #byte 0x02 sent successfully to target
16:30:22:071 : #byte 0xFD sent successfully to target
16:30:22:075 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:22:076 : #ack Received response from target: 0x79
16:30:22:076 : Received 5 data bytes from target : 0x030001061f
16:30:22:076 : Sending GetID command and its XOR:
16:30:22:076 : #byte 0x02 sent successfully to target
16:30:22:076 : #byte 0xFD sent successfully to target
16:30:22:077 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:22:077 : #ack Received response from target: 0x79
16:30:22:077 : Received 5 data bytes from target : 0x030001061f
16:30:23:073 : Sending GetID command and its XOR:
16:30:23:073 : #byte 0x02 sent successfully to target
16:30:23:073 : #byte 0xFD sent successfully to target
16:30:23:073 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:23:073 : #ack Received response from target: 0x79
16:30:23:089 : Received 5 data bytes from target : 0x030001061f
16:30:23:090 : Sending GetID command and its XOR:
16:30:23:090 : #byte 0x02 sent successfully to target
16:30:23:090 : #byte 0xFD sent successfully to target
16:30:23:090 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:23:090 : #ack Received response from target: 0x79
16:30:23:090 : Received 5 data bytes from target : 0x030001061f
16:30:24:079 : Sending GetID command and its XOR:
16:30:24:080 : #byte 0x02 sent successfully to target
16:30:24:080 : #byte 0xFD sent successfully to target
16:30:24:085 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:24:085 : #ack Received response from target: 0x79
16:30:24:091 : Received 5 data bytes from target : 0x030001061f
16:30:24:091 : Sending GetID command and its XOR:
16:30:24:092 : #byte 0x02 sent successfully to target
16:30:24:092 : #byte 0xFD sent successfully to target
16:30:24:092 : Wait ends after 1 loop, dataready = 1, delay = 0
16:30:24:092 : #ack Received response from target: 0x79
16:30:24:092 : Received 5 data bytes from target : 0x030001061f
16:30:24:671 : UART PORT CLOSE 
16:30:24:684 : Disconnected from device.

I think the problem on your side is to use the even parity.

Best Regards.

STTwo-32

TDK
Super User
May 8, 2025

Ahh, it's right there in AN2606. Had no idea some chip bootloaders used no parity instead of even.

TDK_0-1746725434516.png

Looks like this is limited to STM32WB0x products, all others use even parity.

 

@STTwo-32 Thanks for chasing that down.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Davide Dalfra
Associate III
May 9, 2025

Hello guys

 

Yes was the parity setting. I used to give this as always parity as on other BL.

 

Thanks all for the support

 

Davide