How to communicate using the STM32WB55 to a PC without any USB connection
I am designing a project using custom hardware that utilises the STM32WB55 to stream ADC values via DMA from which I want to process using a python script for gesture detection. I want to minimise the use of peer to peer communication and omit the use of a USB dongle to a computer for communication. There are not many resources that go into detail regarding how to communicate from the STM32WB55 to a PC as a peripheral as a continuous stream of information. What do I need to do to enable for host to peripheral communication to a computer using this set up if it is possible?