How to recover from NACK on I2C transaction on STM32WB55
- September 16, 2022
- 1 reply
- 6328 views
My STM32WB55 is configured as I2C master and connected to an I2C slave.
My I2C block is configured like this:
I2C->CR1 = 0x01
I2C->CR2 = 0x000A0060 (slave address=0x60 and NBYTES=0x0A)
To start the I2C transaction I2C->CR2.START is set to 1.
I2C communication starts, but at some point the slave send a NACK, this is expected.
Then, my I2C block is stuck, I acknowledge the I2C_ICR_NACKCF flag, then send another START command. I2C block send START command on the bus but never rise the `I2C->ISR.TXIS` flag, it will never send anymore byte on the bus.
An unexpected STOP is send right after the START.
Here I can see a START command is sent on the bus and acked by the slave:
How to recover from a NACK?
Datasheet shows a diagram, if a NACK is received, state is `End` but what does it mean?
stm32wb55rg_reference_manual.pdf, section 32.4.9 I2C master mode
My only workaround for now is to reset the I2C block. I attached the capture made with a Saleae device.
Despite this NACK problem, it works well.