i-cube-lrwan Class B Beacon not Received
Hi Everyone,
Im working on nucleo L053r8 board with sx1276 lora module and i-cube-lrwan expansion software package.
İ manage to do all the functions class A and Class C With TTN.
Class B working but , beacons are rearly receiving.
First Beacon is always successfull and pingslots are working correctly also it can receive downlinks via pingslots.
Please help me.
Thanks.
APP_VERSION: V1.1.0
MW_LORAWAN_VERSION: V2.3.0
MW_RADIO_VERSION: V1.1.0
0s002:temp= 29
###### OTAA ######
###### AppKey: 18:3B:68:EC:86:CA:A7:A9:62:AB:52:ED:A2:ED:88:91
###### NwkKey: 18:3B:68:EC:86:CA:A7:A9:62:AB:52:ED:A2:ED:88:91
###### ABP ######
###### AppSKey: 59:F2:FC:B6:32:57:72:60:46:F1:82:55:08:5A:D9:5F
###### NwkSKey: 53:29:5F:48:9D:EA:FB:A6:F9:42:0A:8F:00:44:24:DB
###### DevEui: 70:B3:D5:7E:D8:00:33:49
###### AppEui: 00:00:00:00:00:00:00:00
###### DevAddr: 27:FD:99:2B
0s075:temp= 29
0s080:TX on freq 868100000 Hz at DR 0
1s603:MAC txDone
6s638:RX_1 on freq 868100000 Hz at DR 0
8s446:MAC rxDone
###### = JOINED = OTAA =====================
###### ========== MCPS-Indication ==========
150s120:temp= 29
150s121:VDDA= 254
150s125:TX on freq 867500000 Hz at DR 0
150s135:SEND REQUEST
151s783:MAC txDone
156s817:RX_1 on freq 867500000 Hz at DR 0
158s131:MAC rxDone
###### ========== MCPS-Confirm =============
###### ========== MCPS-Indication ==========
1729865471s996:RX_BC on freq 869525000 Hz at DR 3
1729865472s159:MAC rxDone
1729865472s158:TX on freq 868500000 Hz at DR 0
###### ========== BC_RECEIVED
1729865473s322:MAC txDone
1729865478s357:RX_1 on freq 868500000 Hz at DR 0
1729865479s506:MAC rxDone
###### ========== MCPS-Confirm =============
Switch to Class B done
###### ========== MCPS-Indication ==========
1729865584s662:temp= 29
1729865584s663:VDDA= 254
1729865584s667:TX on freq 867100000 Hz at DR 0
1729865596s998:temp= 29
1729865599s989:MAC rxTimeOut
1729865599s989:RX_BC on freq 869525000 Hz at DR 3
###### ========== MCPS-Indication ==========
###### ========== BC_NOT_RECEIVED
1729865599s997:temp= 29
###### ========== MCPS-Indication ==========
###### ========== BC_NOT_RECEIVED
1729865610s071:RX_P on freq 869525000 Hz at DR 3
1729865610s075:MAC rxTimeOut
1729865625s430:RX_P on freq 869525000 Hz at DR 3
1729865625s434:MAC rxTimeOut
1729865640s791:RX_P on freq 869525000 Hz at DR 3
1729865640s794:MAC rxTimeOut
1729865656s151:RX_P on freq 869525000 Hz at DR 3
1729865656s155:MAC rxTimeOut