I-CUBE-LRWAN, P-NUCLEO-LRWAN3, LRWAN_NS1, AT_Master Firmware Problem
I have a P-NUCLEO-LRWAN3 and I have downloaded the I-CUBE-LRWAN expansion software.
Using the project "STM32CubeExpansion_LRWAN_V2.1.0 \ Projects \ NUCLEO-L073RZ \ Applications \ LoRaWAN \ LoRaWAN_AT_Master \ STM32CubeIDE \ LRWAN_NS1" and following the procedure indicated on the file "readme.txt" on the VCOM port I cannot send and receive anything. I also tried to use the "LoRaWAN_End_Node / STM32CubeIDE" project but there is no project related to my SX1278 model. Instead the Gateway works perfectly. I've read all the existing documentation but can't get it to work. What i can do?
Thanks
Edit: by enabling DEBUGGER_ON in "sysconf.h" I can see this but I can't send AT commands