Skip to main content
Visitor II
December 11, 2024
Question

LoRaWAN FUOTA class C

  • December 11, 2024
  • 2 replies
  • 805 views

Hey everybody,

I am currently working on a project which involves a firmware update over the air (using the nucleo wl55jc1 board). i have found an example project through the official website (https://www.st.com/en/embedded-software/stm32cubewl.html) and unzipped the file directly onto my c disk and use powershell to execute the scripts. at first i tried the code without changes besides the changes in the se-identity.h file and everything worked fine see the picture below for the ouptut on the serial monitor.

working_classAworking_classA

once i concluded the project worked i tried to change the class from A to C and got the following

IdiotStudent_0-1733927114845.png

i expected to still see the tx sending data. however that just stopped. i did a deep dive into the code but that just got me more confused. its getting me nowhere and i am not sure on how to proceed. i hope you fine people may shine some light on it. i am using chirpstack as networkserver.

2 replies

STTwo-32
Technical Moderator
January 7, 2025

Hello @IdiotStudent 

It may be an issue on the gateway side. Are you sure is not that?

Best Regards.

STTwo-32

Associate
March 24, 2025

Hii, 

 

I also made the same changes and flashed the end node but my program gets stuck on KMS_init function 

 

Could you provide some guidance on this ?

 

Reagrds, 

Suyash