missing header ble.h
Hi, in custom_stm.h, should add manually #include "ble.h" to works
Hi, in custom_stm.h, should add manually #include "ble.h" to works
Hello
I've personally generated a code on the STM32WB using the STM32_WPAN and the P2P server application type. After compilation, everything works fine and no need to add the file manually (using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1). If you have the need to use the ble.h and it is not included, you need to ad it manually.
Best Regards.
STTwo-32
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.