No advertisments from NUCLEO-WB55RG
Hi
I recently received a NUCLEO-WB55RG (the big board, not the USB dongle) and tried installing the demo from the STM32CubeWB repository.
I saw that I need to flash the FUS + Stack first which I did. STM32CubeProg reports
- FUS State: FUS_IDLE
- FUS Status: FUS_NO_ERROR
- FUS Version: V2.2.0.0
- STACK Version: V1.24.0.3
- STACK Address: 0x80D0000
- FUS Operator: v3.1.0
The files I flashed were:
- STM32CubeWB-master\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_BLE_Stack_full_fw.bin
- STM32CubeWB-master\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_FUS_fw.bin
As application I chose the p2pServer application
- STM32CubeWB-master\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pServer\Binary\BLE_p2pServer_reference.hex
When I disconnect the SWD Interface and press the reset button I get the following output (nothing else):
Wireless Firmware version 1.24.0
Wireless Firmware build 3
FUS version 2.2.0
>>== SHCI_SUB_EVT_CODE_READY
>>== SHCI_SUB_EVT_CODE_READY - FUS_FW_RUNNINGNow I assumed this should be enough to at least see the device advertising.
But none of my applications can see the device. I tried the following apps:
- ST BLE Sensor
- SiConnect (Silabs)
- nRF Connect (nRF)
I do not get a single indication that the device is alive.
What am I missing?