Skip to main content
maborbaa
Associate II
November 13, 2025
Question

NUCLEO-WBA55CG - RTC WUT Fails to Wake MCU from Standby Mode

  • November 13, 2025
  • 2 replies
  • 170 views

Hi everyone,

I'm new to STM32 solutions. My goal is to use the RTC Wake-Up Timer (WUT) to wake the MCU from Standby mode. I'm starting with a simple test:

  • Cold Boot - Program the WUT to wake the MCU in 5 seconds and enter Standby.
  • Warm Boot - Blink an LED, increment a counter (in BKPSRAM), and go back to sleep for 5 more seconds.

The Problem: The MCU enters Standby, but it never wakes up.

I am calculating the WUT for ck_spre (256 Hz) as follows: wakeup_counter = 5 (seconds) * 256 (Hz) = 1280.

HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_RTC_Init();

 if (__HAL_RCC_GET_FLAG(RCC_FLAG_LSERDY) == RESET)
 {
 // LSE FAILED!
 while (1)
	{
	 //(error)
	 HAL_GPIO_WritePin (LED_RED_GPIO_Port, LED_RED_Pin, GPIO_PIN_SET);
	 HAL_Delay (100);
	 HAL_GPIO_WritePin (LED_RED_GPIO_Port, LED_RED_Pin, GPIO_PIN_RESET);
	 HAL_Delay (100);
	}
 }

 uint32_t time_wkp_seg = 5;
 uint32_t wakeup_counter = time_wkp_seg * 256;

 if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF) != RESET)
 {
 // 1. Woke up from Standby

 // 2. Get the state (e.g., a counter)
 uint32_t wake_count = HAL_RTCEx_BKUPRead (&hrtc, RTC_BKP_DR0);
 wake_count++;

 // 3. Execute the wake-up task
 HAL_GPIO_WritePin (LED_GREEN_GPIO_Port, LED_GREEN_Pin, GPIO_PIN_SET); // Turn on LED
 HAL_Delay (50); // Keep it on for 50ms (to be visible)
 HAL_GPIO_WritePin (LED_GREEN_GPIO_Port, LED_GREEN_Pin, GPIO_PIN_RESET); // Turn off LED

 // 4. Save the new state
 HAL_RTCEx_BKUPWrite (&hrtc, RTC_BKP_DR0, wake_count);
 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
 HAL_RTCEx_SetWakeUpTimer_IT (&hrtc, wakeup_counter, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 0);
 }
 else
 {
 // 5. It's a "cold" boot

 // 6. Save the initial state
 HAL_RTCEx_BKUPWrite (&hrtc, RTC_BKP_DR0, 0); // Start counter
 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
 HAL_RTCEx_SetWakeUpTimer_IT (&hrtc, wakeup_counter, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 0);
 }

 // --- Safety Clear BEFORE sleeping ---
 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);// Clear the RTC flag
 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SBF); // Clear PWR flags

 HAL_PWR_EnterSTANDBYMode ();

 

2 replies

Technical Moderator
November 17, 2025

hello @maborbaa 
I suspect that the issue is caused by an incorrect configuration.
You can refer to this firmware example, which implements the RTC and standby mode, to base your project on it.
Since you are new to STM32 solutions, you can consult this Wiki to learn more about low-power modes.
BR
Gyessine

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Jtron.11
Senior
December 6, 2025

Hi @maborbaa ,

I learn that I need to enable the wakeup pin HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN7_HIGH_3);

for my RTC to wake up.

Also check your source of waking up.  Look like you are using RTC.  Are you running form LSE external 32KHz?

You can use this example as a reference since I have it working for my custom STM32WBA52 board.