Nulceo WB55 Example not waking up from stop mode from LPUART
I have referred to the Example project "LPUART_WakeUpFromStop_Init". Configured an LP-UART in interrupt mode with a baud rate of 9600, Stop bit 1, Parity None, and enabled the HSI clock source for it. When the device enters the stop mode, try to send a character to wake it. But it is not all waking up.
We need to try this on Nulceo WB55 evaluation board. Once it works, we need to use it on our product which uses the uC STM32WB55VGQ.