Skip to main content
Associate
September 10, 2025
Question

Powering NUCLEOWB55RG Externally with 3.3V, How to Program it?

  • September 10, 2025
  • 1 reply
  • 330 views

Hi I have a PCB board based off of NUCLEOWB55RG board. I am planning to power it externally (3.3V regulator and Lipo battery) but I also want to program it. How can I disable the onboard regulator to program it with USB? Or can I program it using the J-Link board instead? 

I ran a test by removing the JP1 jumper, the 3.3V output remains 0. However, the ST-LINK doesnt work when I program using CUBEIDE. 

How can I proceed with this?

1 reply

TDK
Super User
September 10, 2025

Powering the board shouldn't add additional complications here. Attach the programmer to the board and it should be able to connect if you have it wired correctly. I recommend using a standard programming header/pinout and an official programmer. The programmer typically doesn't provide power.

GND/SWDIO/SWCLK need connected at a minimum. Recommended VDD/NRST as well.

"If you feel a post has answered your question, please click ""Accept as Solution""."
fshaikh98Author
Associate
September 10, 2025

What type of programmers would you recommend for this board? A segger J-Link or do I have cheaper options? Intention is for this board to be used for commercial purposes, large scale manufacturing later on

STTwo-32
Technical Moderator
September 29, 2025

Hello @fshaikh98 

The best way is to connect and program using the USB or USART and following the recommendations of AN2606.

Best Regards.

STTwo-32