Skip to main content
Associate II
September 9, 2024
Solved

Receive sensitivity of GFSK modem on STM32WL55

  • September 9, 2024
  • 1 reply
  • 735 views

The STM32WL5x Datasheet mentions the RX Sensitivity of the Radio Modem for both 2-FSK and LoRa modulation (see image below) but makes no mention of GFSK, GMSK or BPSK

MoralkaraLynn_0-1725865626245.png

What are the receive sensitivity values for these modulation schemes?

Best answer by STTwo-32

Hello @MoralkaraLynn and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The sub-GHz radio implemented on the STM32WL5x support Transmission and Reception using the LoRa and the 2-FSK modulations. But it supports only the Transmission for the 2-MSK and BPSK modulation. So, no reception for GMSK, MSK and BPSK. For the GFSK, it is mentioned on the 2-FSK (FSK & GFSK). 

Then, RX sensitivity parameter should be available only For LoRa, FSK and GFSK.

Best Regards.

STTwo-32

1 reply

STTwo-32
STTwo-32Best answer
Technical Moderator
September 9, 2024

Hello @MoralkaraLynn and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The sub-GHz radio implemented on the STM32WL5x support Transmission and Reception using the LoRa and the 2-FSK modulations. But it supports only the Transmission for the 2-MSK and BPSK modulation. So, no reception for GMSK, MSK and BPSK. For the GFSK, it is mentioned on the 2-FSK (FSK & GFSK). 

Then, RX sensitivity parameter should be available only For LoRa, FSK and GFSK.

Best Regards.

STTwo-32