Skip to main content
Associate II
December 5, 2025
Solved

Recovering STM32WB05KZ When SWD Is Disabled by BLE Firmware

  • December 5, 2025
  • 1 reply
  • 876 views

Hello,

I am using an STM32WB05KZ on a custom PCB. Initially, I was able to program it normally via SWD using STM32CubeProgrammer, but after uploading a BLE Beacon example, I can no longer connect to the MCU.

CubeProgrammer now shows:

  • Error: Unable to get core ID

  • Error: ST-LINK error (DEV_TARGET_CMD_ERR)

  • No STM32 target found

My Hardware Setup

  • Custom PCB using STM32WB05KZ

  • SWDIO, SWCLK, RST, VDD, GND routed through through-hole pads

  • ST-LINK V2 firmware: V2J46M33

  • Operating voltage: 3.21 V

  • SWD frequency tested from 4 MHz down to 100 kHz

  • Tried Normal, Hotplug, and Under Reset modes

  • Tried holding RESET while connecting → no success

My Situation

After flashing the BLE firmware, SWD stopped responding completely.
It seems the firmware reconfigured the SWD pins early or put the device into DeepStop, which disables SWD access.

I saw advice suggesting to force the chip into the UART bootloader by pulling PA10 HIGH and resetting.
However, since I designed a custom PCB (not the NUCLEO-WB05KZ), I manually tie PA10 to VDD and then reset, but SWD still does not reconnect.

I have attached the PCB pinout and SWD/UART wiring for reference (in the actual forum post).

Requested Help

  1. How can I recover the STM32WB05KZ and re-enable SWD?

  2. Is there a recommended recovery procedure for WB devices stuck after BLE firmware or DeepStop?

  3. Does the WB05KZ support a boot pin (similar to BOOT0) to force the system bootloader?

  4. How can I prevent future BLE examples from disabling SWD or forcing STOP mode?

Any guidance from ST engineers or community experts would be greatly appreciated.

Thank you.

pradeepaan_0-1764911571039.jpegpradeepaan_1-1764911588608.jpegpradeepaan_2-1764911602089.jpegpradeepaan_3-1764911620591.jpeg

 

pradeepaan_4-1764911644856.pngpradeepaan_5-1764911706836.pngpradeepaan_6-1764911735365.png

 




Best answer by TDK

See AN2606 for ways to boot up into the bootloader. Once in the bootloader, SWD will work.

TDK_0-1764943001849.png

 

If none of those are feasible, you will need to try to hit "Connect" on STM32CubeProgrammer right after power is applied and before the firmware goes into low power mode. Depending on your program, this may or may not be possible.

 

Those are the only options.

1 reply

TDK
TDKBest answer
Super User
December 5, 2025

See AN2606 for ways to boot up into the bootloader. Once in the bootloader, SWD will work.

TDK_0-1764943001849.png

 

If none of those are feasible, you will need to try to hit "Connect" on STM32CubeProgrammer right after power is applied and before the firmware goes into low power mode. Depending on your program, this may or may not be possible.

 

Those are the only options.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Associate II
December 8, 2025

Hi TDK

Thank you so much.It's working.

vijay