Since updating STM32CubeIde STM32WB fails after making changes
Ever since being forced to update STM32CubeIde, every time a change is made to the .ioc file and the code is regenerated the following errors show up.
app_ble.c
/**
* Write the BD Address
*/
p_bd_addr = BleGetBdAddress();
ret = aci_hal_write_config_data(CONFIG_DATA_PUBLIC_ADDRESS_OFFSET, CONFIG_DATA_PUBLIC_ADDRESS_LEN, (uint8_t*) p_bd_addr);
if (ret != BLE_STATUS_SUCCESS)
{
APP_DBG_MSG(" Fail : aci_hal_write_config_data command - CONFIG_DATA_PUBLIC_ADDRESS_OFFSET, result: 0x%x \n", ret);
}
else
{
APP_DBG_MSG(" Success: aci_hal_write_config_data command - CONFIG_DATA_PUBLIC_ADDRESS_OFFSET\n");
APP_DBG_MSG(" Public Bluetooth Address: %02x:%02x:%02x:%02x:%02x:%02x\n",p_bd_addr[5],p_bd_addr[4],p_bd_addr[3],p_bd_addr[2],p_bd_addr[1],p_bd_addr[0]);
}
CONFIG_DATA_PUBLIC_* needs to be changed to CONFIG_DATA_RANDOM_*
case ACI_HAL_WARNING_VSEVT_CODE:
{
aci_hal_warning_event_rp0 *p_warning_event;
p_warning_event = (aci_hal_warning_event_rp0 *)p_blecore_evt->data;
UNUSED(p_warning_event);
APP_DBG_MSG(">>== ACI_HAL_WARNING_VSEVT_CODE\n");
APP_DBG_MSG("Warning Type = 0x%02X\n", p_warning_event->Warning_Type);
/* USER CODE BEGIN ACI_HAL_WARNING_VSEVT_CODE */
//
/* USER CODE END ACI_HAL_WARNING_VSEVT_CODE */
break;
}Apparently, ACI_HAL_WARNING_VSEVT_CODE is no longer a thing.
../STM32_WPAN/App/app_ble.c: In function 'SVCCTL_App_Notification':
../STM32_WPAN/App/app_ble.c:673:14: error: 'ACI_HAL_WARNING_VSEVT_CODE' undeclared (first use in this function); did you mean 'ACI_HAL_FW_ERROR_VSEVT_CODE'?
673 | case ACI_HAL_WARNING_VSEVT_CODE:
| ^~~~~~~~~~~~~~~~~~~~~~~~~~
| ACI_HAL_FW_ERROR_VSEVT_CODE
../STM32_WPAN/App/app_ble.c:673:14: note: each undeclared identifier is reported only once for each function it appears in
../STM32_WPAN/App/app_ble.c:675:11: error: unknown type name 'aci_hal_warning_event_rp0'; did you mean 'aci_hal_fw_error_event_rp0'?
675 | aci_hal_warning_event_rp0 *p_warning_event;
| ^~~~~~~~~~~~~~~~~~~~~~~~~
| aci_hal_fw_error_event_rp0
../STM32_WPAN/App/app_ble.c:677:34: error: 'aci_hal_warning_event_rp0' undeclared (first use in this function); did you mean 'aci_hal_fw_error_event_rp0'?
677 | p_warning_event = (aci_hal_warning_event_rp0 *)p_blecore_evt->data;
| ^~~~~~~~~~~~~~~~~~~~~~~~~
| aci_hal_fw_error_event_rp0
../STM32_WPAN/App/app_ble.c:677:61: error: expected expression before ')' token
677 | p_warning_event = (aci_hal_warning_event_rp0 *)p_blecore_evt->data;
#define CFG_BLE_MAX_ADD_EATT_BEARERS (4)
../STM32_WPAN/App/app_ble.c: In function 'APP_BLE_Init':
../Core/Inc/app_conf.h:360:49: warning: excess elements in struct initializer
360 | #define CFG_BLE_MAX_ADD_EATT_BEARERS (4)
| ^
../STM32_WPAN/App/app_ble.c:302:10: note: in expansion of macro 'CFG_BLE_MAX_ADD_EATT_BEARERS'
302 | CFG_BLE_MAX_ADD_EATT_BEARERS
| ^~~~~~~~~~~~~~~~~~~~~~~~~~~~
../Core/Inc/app_conf.h:360:49: note: (near initialization for 'ble_init_cmd_packet.Param')
360 | #define CFG_BLE_MAX_ADD_EATT_BEARERS (4)
| ^
../STM32_WPAN/App/app_ble.c:302:10: note: in expansion of macro 'CFG_BLE_MAX_ADD_EATT_BEARERS'
302 | CFG_BLE_MAX_ADD_EATT_BEARERS
What am I doing wrong, do I need to do something, so it generates the code correctly?
Kindest regards