STM32 WB55RG sudden fail
-------------------------------------------
Board: STM32 WB55RG
OS: Ubuntu 25.10 questing
Kernel: x86_64 Linux 6.17.0-6-generic
STMCubeProgrammer Version: v2.21.0
-------------------------------------------
I recently noticed that my board was not being flashed with the following error:
No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug Authentication
I tried connecting the board using the STM32CubeProgrammer and while the board is recognized correctly by ST-LINK (the serial number shows up) I still cannot connect the board because of the same error.
When the issues started to occur, I was using my board normally with the usual code running when the board suddenly stopped providing power to the pins; I was using the board to power an external device using the 5 V pin, but my meter only measures about 1 V across the 5 V pin and GND and 200 mV across 3.3 V and GND.
Connecting the board still shows bicolor LED blinking and the LED 4 is always on which I was told it indicates over currents somewhere on the board.
The board also has this fail.txt file when connected using USB:
The interface firmware FAILED to reset/halt the target MCU
I believe the board might be unrecoverable, but I would like to know if anyone has ever had similar issues, if it's common or what might be the causes.
Thanks in advance.