Skip to main content
Associate
August 21, 2025
Solved

STM32CubeIDE 1.19.1 + STM32CubeWL build fails on new project: 'ResponseTimeout' member not found

  • August 21, 2025
  • 1 reply
  • 834 views

Hello,

I'm having trouble building a LoRaWAN project targeting the STM32WLE5JCI6. The same error occurs even on a clean, newly created project, which leads me to believe there might be a compatibility issue between the IDE and the software package.

■ The error I'm facing:

../Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c: In function 'ProcessRadioRxDone':
../Middlewares/Third_Party/LoRaWAN/Mac/LoRaMac.c:1650:40: error: 'McpsIndication_t' {aka 'struct sMcpsIndication'} has no member named 'ResponseTimeout'

This error indicates that LoRaMac.c is trying to access the ResponseTimeout member of the McpsIndication_t struct, but the corresponding LoRaMac.h file lacks that definition.

■ My setup:

  • Target MCU: STM32WLE5JCI6

  • STM32CubeIDE Version: 1.19.1 (Clean install from the official website)

  • STM32CubeWL Package: Latest version (Installed via the IDE's package manager)

■ Steps I have already taken:

  1. Cleanly reinstalled both STM32CubeIDE and the STM32CubeWL package.

  2. Deleted the old project and workspace, then created a new project from scratch in a new workspace.

  3. The project was generated with default settings, with only the LoRaWAN stack enabled.

■ My findings:

  • The LoRaMac.h file within my new project folder does not contain the definition for the ResponseTimeout member.

  • The latest LoRaMac-node repository on GitHub, however, does include this definition.

■ My question:

Is this a known issue with the combination of the latest STM32CubeIDE and STM32CubeWL package? If you know of a solution, your assistance would be greatly appreciated.

I am using an AI to formulate this question.
Thank you.


Best answer by STTwo-32

Hello @R_JPstudent 

If you select LoRaWAN Link Layer version 1.0.3, the ResponseTimeout item is not included, and the error occurs. A possible work-around is to comment-out the #if/#endif in the code snippet (at line 1518 in LoRaMacInterfaces.h file). So ResponseTimeout is always included regardless of LoRaWAN Link Layer. If you do this, you will need to re-do it every time CubeMX generates code and over-writes the change. Also, you can change from LoRaWAN Link Layer specification from 1.0.3 to 1.0.4:

STTwo32_0-1756107919709.png

PS: This is already reported and will be solved on the future. For more details, have a look at this post.

Best Regards.

STTwo-32

1 reply

Ghofrane GSOURI
Technical Moderator
August 21, 2025

Hello @R_JPstudent 

Could you please share your project files ? This will help me better understand your configuration  and assist you more effectively.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
August 25, 2025

Hello Ghofrane,

Thank you for your quick response.

I have attached the project file as requested.

Please let me know if you need any other information.

Thank you for your support.

Best regards,

R

STTwo-32
STTwo-32Best answer
Technical Moderator
August 25, 2025

Hello @R_JPstudent 

If you select LoRaWAN Link Layer version 1.0.3, the ResponseTimeout item is not included, and the error occurs. A possible work-around is to comment-out the #if/#endif in the code snippet (at line 1518 in LoRaMacInterfaces.h file). So ResponseTimeout is always included regardless of LoRaWAN Link Layer. If you do this, you will need to re-do it every time CubeMX generates code and over-writes the change. Also, you can change from LoRaWAN Link Layer specification from 1.0.3 to 1.0.4:

STTwo32_0-1756107919709.png

PS: This is already reported and will be solved on the future. For more details, have a look at this post.

Best Regards.

STTwo-32