STM32CubeProgrammer fatal Java error with LSM100A (STM32WLE5CC) and ST-Link V2
Hello,
i try to program LSM100A ( STM32WLE5CC ) .
i can connect but can't program an elf file : error fail to erase memory, then cube programmer crashed.
thank you for support
logs :
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0x000078ae2276d917, pid=43070, tid=0x000078ae31bff6c0
#
# JRE version: OpenJDK Runtime Environment (8.0_382-b06) (build 1.8.0_382-b06)
# Java VM: OpenJDK 64-Bit Server VM (25.382-b06 mixed mode linux-amd64 compressed oops)
# Problematic frame:
# C [libCubeProgrammer_API.so+0x16d917] checkDeviceConnection+0xa7
#
# Failed to write core dump. Core dumps have been disabled. To enable core dumping, try "ulimit -c unlimited" before starting Java again
#
# An error report file with more information is saved as:
# /home/dam/STM32CubeProgrammer/bin/hs_err_pid43070.log
#
# If you would like to submit a bug report, please visit:
# https://bell-sw.com/support
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
STM32CubeProgrammer/bin/STM32CubeProgrammer : ligne 5 : 43070 Abandon (core dumped) GDK_BACKEND=x11 "$DIR"/jre/bin/java -Djdk.gtk.version=2 -jar "$DIR/STM32CubeProgrammerLauncher" 2> /dev/null