STM32F429IGT6 Dual Bank OTA updates
Hi folks,
I am trying to implement a dual bank OTA system on my STM32F429IGT6 using DBM1 and BFB2 in the STMCubeProgrammer, but I'm having trouble booting into the second flash region (which I will call app_b from now on, along with app_a for the first flash region). By my logic, each app will have 512KB of flash memory, so app_a will start at 0x08000000, and app_b will start at 0x08080000. Through some online digging, I saw that having one linker script per app is what I should be doing, with each app's flash being its address that I mentioned before, but then set the app_b vector table offset to 0x00080000, so theoretically app_b can start at 0x08080000 because that's the result from the OR operation of 0x08000000 and 0x00080000. So here is my normal testing routine:
Build App_A, note version number --> generate a .bin file through a post build command
Flash App_A with start address 0x08000000 in the CubeProgrammer
Append Version Number to see change
Build App_B --> generate .bin file
Flash App_B with start address 0x08080000 in the CubeProgrammer
*From this point BFB2 would still be set to 0, and I can reset my board and it boots up fine to App_A*
Enable BFB2 (BFB2->1)
Restart board, but no response at all
Disable BFB2 (BFB2->0)
Restart board, boots to App_A fine
Essentially its the same file just besides the version number, which is just a const char*, the origin address in the linker, and the vect table offset. Any help would be appreciated, thank you!