STM32WB set CPU sleep for low power consumption
Hi,
I use an STM32WB chipset for my device and my application reads sensor data and sends over the BLE when the device is connected. When the device gets disconnected then after 30 seconds it should STOP BLE advertisement and RF also, go to CPU sleep and wait for GPIO interrupt to wake. I have tested a development for CPU sleep when BLE is not enabled and it is working fine, The CPU goes to sleep and wakes on GPIO interrupt, but after enabling the BLE, it is not going to sleep.
void cpu_sleep(){
if(cpu_running_status == BA_ENABLE){
cpu_running_status = BA_DISABLE;
HAL_SuspendTick();
LL_PWR_SetPowerMode( LL_PWR_MODE_STOP2 );
LL_LPM_EnableDeepSleep( ); /**< Set SLEEPDEEP bit of Cortex System Control Register */
__WFI();
}
}
void cpu_wakeup(){
if(cpu_running_status == BA_DISABLE){
cpu_running_status = BA_ENABLE;
HAL_ResumeTick();
HAL_Delay(10);
}
}
Here I have added the snippet of code which is working fine without BLE