[STM32WB55] Flash operations without Wireless Stack and without using CPU2
Hello!
I have a question about doing flash operations without the BLE wireless stack firmware being present in STM32. As it seems from the examples, the flash operations requires to notify the CPU2. For example, when doing flash erase, the CPU2 will have to be notified first in order to continue with it. But since wireless stack is not present, a HardFault is encountered after notifying, because no wireless stack is present. The question is now, if it is possible to do flash operations without having to notify CPU2, and thus not needing to have the wireless stack present in STM32?
If the answer is yes, then where could one find an example of doing so?