STM32WB55: What is a "normal" delay on flash erase during advertisement
I know that flash erase during BLE activity is an issue with that controller and a lot of notification/semaphore stuff needs to be build around it. But measuring my implementation including the later today, it looks a lot more horrible than I imagined.
If I have BLE Advertisement (no connection open!) on with Advertising_Interval_Min = 1800 Advertising_Interval_Max = 4000, deleting one block of flash takes nearly 1 second (~815ms). If I stop Advertisement afterwards, it remains the same. Only if I disable the stack completely, or did not yet start the first advertisement, I get back to the 25ms ballpark from the HW itself.
Is this really the delay I will now have to find a way to work around, or should I have a look at my flash erase routine again.