Solved
STM32WB55CG Zigbee write sensor value
- November 13, 2024
- 1 reply
- 2340 views
Hi,
i want to send sensor values from my STM to my Homeassistant via zigbee.
Therefore I have configured a temperature sensor cluster at one endpoint and because my device should also control LEDs, I have an onoff cluster.
I have tried to send my sensordata with
ZbZclAttrIntegerWrite(zigbee_app_info.temperature_meas_server_2, ZCL_WC_MEAS_ATTR_MEAS_VAL, 12);
As a start, i places this line into the "onOff_server_1_on" function, so that I could see, when I send an on command from my Homeassistant, the temperature gets send, which also works fine.
However, I tried calling the function with an external set routine cyclic (every 10s) from my ISR, which did not work and caused my processor to crash. Can anybody see a reason for that? I also attachted my app_zigbee.c here.
Thanks