Skip to main content
Associate
September 9, 2024
Solved

STM32WB55CGUX (48 pin) Touch Sense Controller (TSC) capabilities

  • September 9, 2024
  • 1 reply
  • 1542 views

Hi,

we are looking for a microcontroller fitting the following features:

  • 1MB Flash
  • 256kB RAM 
  • BLE
  • 48 pins (non BGA)
  • Touch Sense Controller (TSC)
  • Active and stock

We pointed to STM32WB55CGUX but we see the following note on the datasheet STM32WB55C (page 48):

eesyES_0-1725888143837.png

Does that mean that we do not have any available TSC sensing channel on the QFN48 version? Or just that the number of channels is limited? Checking with the Pinout & Configuration tool of the STM32CubeIDE, we do not see any available TSC port at any pin of the STM32WB55CGU6TR (48 pins QFN version).

eesyES_2-1725888839022.png

Instead, we have selected the STM32WBA55CGU6X one, to the detriment of RAM, being 128kB instead of 256kB. If you have any microcontroller suggestion besides this one fitting the main requirements, we would really appreciate it.

Thanks in advance.

Regards,

eesy-ES team.

 

 

Best answer by STTwo-32

For the body proximity detection, you can configure it using the TSC.

In AN5105, we explain where to locate information in chapter 5.2 (signal Threshold):
 
..
,MyTKeys[Index].p_Param->ProxInTh
,MyTKeys[Index].p_Param->ProxOutTh
..
ProxInTh and ProxOutTh are defined for proximity detection feature only, when TSLPRM_USE_PROX = 1.
..
 
References are:
UM1913, Developing applications on STM32Cube with STMTouch® touch sensing library
* 3.11.6 PROXIMITY state
AN4316, Tuning a STMTouch-based application
* 4.2.3 Proximity
 
 
Regarding Prox feature:
=======================
 
On tsl_conf.h, these defines are involved:
 
#define TSLPRM_USE_PROX ()
#define TSLPRM_TKEY_PROX_IN_TH ()
#define TSLPRM_TKEY_PROX_OUT_TH ()
#define TSLPRM_DEBOUNCE_PROX ()
 
On tsl_type.h, StateId to used are:
 
  // Proximity states
  TSL_STATEID_PROX               = 6,  /**<  6 - Object is in Proximity */
  TSL_STATEID_DEB_PROX           = 7,  /**<  7 - Object is in Debounce Proximity from Release state */
  TSL_STATEID_DEB_PROX_DETECT    = 8,  /**<  8 - Object is in Debounce Proximity from Detect state */
  TSL_STATEID_DEB_PROX_TOUCH     = 9,  /**<  9 - Object is in Debounce Proximity from Detect state */
 
Using default TSL/TSC operating mode:
 
/** Proximity detection usage (0=No, 1=Yes)
*/
#define TSLPRM_USE_PROX (1)
/** TouchKeys Proximity state input threshold (range=0..255)
  - Enter Proximity state if delta is above
*/
#define TSLPRM_TKEY_PROX_IN_TH (6)
/** TouchKeys Proximity state output threshold (range=0..255)
  - Exit Proximity state if delta is below
*/
#define TSLPRM_TKEY_PROX_OUT_TH (4)
/** Proximity state debounce in samples unit (range=0..63)
  - A Low value will result in a higher sensitivity during the Proximity detection but with less noise filtering.
  - A High value will result in improving the system noise immunity but will increase the system response time.
*/
#define TSLPRM_DEBOUNCE_PROX (2)
 
Regarding usual recommendation:
===============================
 
(Extracted from old documentations....)
 
The following factors influence proximity sensitivity:
● Capacitive system ground
– A battery supplied portable system versus a well-grounded system offer different system sensitivity
● Electrode (CX)
– Size: a bigger the electrode size increases the coupling between the user and the electrode and thus improves the sensitivity.
– Shape: the shape of the electrode is directly linked to the detection area expected for the application.
– Ground and supply proximity to sensor and tracks.
– Route and distance between electrodes and proximity sensor.
● Sampling capacitor (CS)
– Increasing the CS capacitor increases the resolution of the CX measurement.
● Panel
– Materials and thickness can modify the sensitivity. The better the dielectric value, the better the sensitivity of the sensors (glass is better than plastic).
– Avoid air gaps between the sensor and the overlay material. For example, use a spring with a conductive surface pressing against the overlay where big air gaps exist or attach the touch pad directly to an overlay using non-conductive glue/double-sided tape.
● Power supply
– Variation in the power supply level can disrupt the sensor measurement and cause unwanted proximity detection.
● Temperature
– Temperature variations have an effect on the proximity sensor measurement 
Special care should be taken of the above factors to ensure stability of the sensor systems. Increasing the sensitivity of the sensor excessively (by increasing the electrode size or the CS) can cause an unstable sensor system and trigger unwanted proximity detection.
 
Best Regards.
STTwo-32

 

 

1 reply

STTwo-32
Technical Moderator
September 9, 2024

Hello @eesy-ES and welcome to the ST Community :smiling_face_with_smiling_eyes:.

The TSC is not supported by the STM32WB55/35 with QFPN48 Package. 

For the STM32WBA55, your choice is the most compatible with the needs you have specified on your post (maximum RAM size available for the STM32WBA55 is 128 Kbytes). the STM32WBA55CGU6TR will be the best choice since you can use both NUCLEO-WBA55CG and STM32WBA55G-DK1 for evaluation before Board conception, Mass Market, ...

Best Regards.

STTwo-32

eesy-ESAuthor
Associate
September 9, 2024

Thanks for the quick reply.

Another question regarding this Touch Sense Controller is if we can make it to work for body proximity detection, instead of just for touch little keys. If so, could you lead us to documentation where to know more about that? 

Best Regards,

eesy-ES team.

STTwo-32
STTwo-32Best answer
Technical Moderator
September 9, 2024

For the body proximity detection, you can configure it using the TSC.

In AN5105, we explain where to locate information in chapter 5.2 (signal Threshold):
 
..
,MyTKeys[Index].p_Param->ProxInTh
,MyTKeys[Index].p_Param->ProxOutTh
..
ProxInTh and ProxOutTh are defined for proximity detection feature only, when TSLPRM_USE_PROX = 1.
..
 
References are:
UM1913, Developing applications on STM32Cube with STMTouch® touch sensing library
* 3.11.6 PROXIMITY state
AN4316, Tuning a STMTouch-based application
* 4.2.3 Proximity
 
 
Regarding Prox feature:
=======================
 
On tsl_conf.h, these defines are involved:
 
#define TSLPRM_USE_PROX ()
#define TSLPRM_TKEY_PROX_IN_TH ()
#define TSLPRM_TKEY_PROX_OUT_TH ()
#define TSLPRM_DEBOUNCE_PROX ()
 
On tsl_type.h, StateId to used are:
 
  // Proximity states
  TSL_STATEID_PROX               = 6,  /**<  6 - Object is in Proximity */
  TSL_STATEID_DEB_PROX           = 7,  /**<  7 - Object is in Debounce Proximity from Release state */
  TSL_STATEID_DEB_PROX_DETECT    = 8,  /**<  8 - Object is in Debounce Proximity from Detect state */
  TSL_STATEID_DEB_PROX_TOUCH     = 9,  /**<  9 - Object is in Debounce Proximity from Detect state */
 
Using default TSL/TSC operating mode:
 
/** Proximity detection usage (0=No, 1=Yes)
*/
#define TSLPRM_USE_PROX (1)
/** TouchKeys Proximity state input threshold (range=0..255)
  - Enter Proximity state if delta is above
*/
#define TSLPRM_TKEY_PROX_IN_TH (6)
/** TouchKeys Proximity state output threshold (range=0..255)
  - Exit Proximity state if delta is below
*/
#define TSLPRM_TKEY_PROX_OUT_TH (4)
/** Proximity state debounce in samples unit (range=0..63)
  - A Low value will result in a higher sensitivity during the Proximity detection but with less noise filtering.
  - A High value will result in improving the system noise immunity but will increase the system response time.
*/
#define TSLPRM_DEBOUNCE_PROX (2)
 
Regarding usual recommendation:
===============================
 
(Extracted from old documentations....)
 
The following factors influence proximity sensitivity:
● Capacitive system ground
– A battery supplied portable system versus a well-grounded system offer different system sensitivity
● Electrode (CX)
– Size: a bigger the electrode size increases the coupling between the user and the electrode and thus improves the sensitivity.
– Shape: the shape of the electrode is directly linked to the detection area expected for the application.
– Ground and supply proximity to sensor and tracks.
– Route and distance between electrodes and proximity sensor.
● Sampling capacitor (CS)
– Increasing the CS capacitor increases the resolution of the CX measurement.
● Panel
– Materials and thickness can modify the sensitivity. The better the dielectric value, the better the sensitivity of the sensors (glass is better than plastic).
– Avoid air gaps between the sensor and the overlay material. For example, use a spring with a conductive surface pressing against the overlay where big air gaps exist or attach the touch pad directly to an overlay using non-conductive glue/double-sided tape.
● Power supply
– Variation in the power supply level can disrupt the sensor measurement and cause unwanted proximity detection.
● Temperature
– Temperature variations have an effect on the proximity sensor measurement 
Special care should be taken of the above factors to ensure stability of the sensor systems. Increasing the sensitivity of the sensor excessively (by increasing the electrode size or the CS) can cause an unstable sensor system and trigger unwanted proximity detection.
 
Best Regards.
STTwo-32