Skip to main content
Associate
August 21, 2025
Solved

STM32WB55RGV6 – BLE stack stopped working after switching projects (even old examples fail)

  • August 21, 2025
  • 7 replies
  • 1120 views

Hello,

I am working with an STM32WB55RGV6 on a custom board powered by battery (always connected).

I successfully ran the Proximity example (non-RTOS) with BLE stack before, but after I worked on another project that used BLE stack + FreeRTOS, the BLE stack no longer works — even the old Proximity example stopped advertising.

Current status

  • FUS Info (read via CubeProgrammer):

    • FUS State: FUS_IDLE

    • FUS Status: FUS_NO_ERROR

    • FUS Version: v2.1.0.0

    • Wireless Stack Version: v1.23.0.3

    • Stack address: 0x080D0000

    • FUS Operator: v3.1.0

  • Option Bytes:
    • RDP = 0xAA

    • SFSA = 0xD0 (0x080D0000)

  • Boot config (nBOOT0, nSWBOOT0) 

     

I already tried:

  • Upgrading FUS and reinstalling BLE stack.

  • Mass erase + reflashing the Proximity example.

Result: No advertising, no BLE activity.

What is the recommended way to fully recover BLE stack on a custom board (always battery powered) after using another project?

Best answer by OussamaBousselmi

Hello, 
it turns out that a full power cycle is mandatory after operations involving FUS, wireless stack installation/removal, or related option-byte changes on the STM32WB series. A simple reset is not enough to properly reinitialize the system.
In my case, I forced the battery to discharge and tested it again, and it works perfectly.
Thank you.

Best regards,
Oussama.

7 replies

STTwo-32
Technical Moderator
August 21, 2025

Aslema @OussamaBousselmi W Marahba fel ST Community.

I suggest you to update the FUS and Stack using the .bin files available on the STM32CubeWB V1.23.0 and the STM32CubeProgtammer V2.20.0. After that, Click on the ´Start wireless stack’ button of the STM32CubeProgrammer. Finally, go and upload your application.

Liltek zina.

STTwo-32

Associate
August 22, 2025

Aslema @STTwo-32, aychek :D


thank you for your quick response.
Unfortunately, I have already tried that, but it does not solve the problem.

FilipKremen
ST Employee
August 22, 2025

Hello,

can you please try to debug the project? Any hardfaults?

Also, can you please try to delete the stack before installing a new one?

Thank you.

 

Best regards,

Filip Kremen

Remy ISSALYS
Technical Moderator
August 22, 2025

Hello,

Can you please share the SBRV option byte value? 

Best Regards

Associate
August 22, 2025

Hello,

Thanks for your follow-up.

@FilipKremen 
I’ve already deleted the stack and reinstalled a fresh one, but the issue remains unchanged. There are no hardfaults, and the function Adv_Request() is still never reached during execution.

@Remy ISSALYS 
Regarding your request, the SBRV option byte value is set to 0x34000.

Please let me know if there’s anything else I should check or modify.

Best regards,
Oussama.

OussamaBousselmiAuthorBest answer
Associate
August 25, 2025

Hello, 
it turns out that a full power cycle is mandatory after operations involving FUS, wireless stack installation/removal, or related option-byte changes on the STM32WB series. A simple reset is not enough to properly reinitialize the system.
In my case, I forced the battery to discharge and tested it again, and it works perfectly.
Thank you.

Best regards,
Oussama.

Associate
August 26, 2025

Hello again,
is there another way to perform a full power cycle without draining/disconnecting the battery? 

Best regards,
Oussama.