Skip to main content
Associate III
November 17, 2025
Question

STM32WB5MMG and USB

  • November 17, 2025
  • 1 reply
  • 157 views

Hi,

I'm working with an STM32WB5MMG. I need to use both USB and BLE. I see that there are some threads opened about problems regarding the use of both USB and BLE in the same project due to the HSI48. However, I added LL_HSEM_1StepLock(HSEM, 5) to prevent the CPU2 to disable the HSI48 oscillator when it does not use anymore the RNG IP. It was working until I add all the peripheral. I report my main code.

Someone has suggestion?

Thanks.

int main(void)
{

 /* USER CODE BEGIN 1 */
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 /* Config code for STM32_WPAN (HSE Tuning must be done before system clock configuration) */
 MX_APPE_Config();

 /* USER CODE BEGIN Init */
 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* Configure the peripherals common clocks */
 PeriphCommonClock_Config();

 /* IPCC initialisation */
 MX_IPCC_Init();

 /* USER CODE BEGIN SysInit */

 //NB: to use USB and BLE you must add this line
 /**
	* This prevents the CPU2 to disable the HSI48 oscillator when
	* it does not use anymore the RNG IP
 */
 LL_HSEM_1StepLock(HSEM, 5);

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_RTC_Init();
 MX_I2C1_Init();
 MX_LPUART1_UART_Init();
 MX_SPI1_Init();
 MX_CRC_Init();
 MX_USB_Device_Init();
 MX_RF_Init();
 /* USER CODE BEGIN 2 */
 /* USER CODE END 2 */

 /* Init code for STM32_WPAN */
 MX_APPE_Init();

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 MX_APPE_Process();

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

 

1 reply

Technical Moderator
November 17, 2025

Hi @matteverze 

I'm not expert in STM32 Wireless products. I suggest you check AN5289 for detailed algorithms and guidelines on managing USB and BLE.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.Best regards,FBL
Associate III
November 19, 2025

Thanks. I found out that the problem is related to the low-power mode. Infact, I had CFG_LPM_SUPPORTED to 1. Do you have any suggestion of how to manage low power mode and USB?

Thanks