Skip to main content
Associate II
October 12, 2024
Solved

STM32WB5MMG LSE clock 32.774 kHz?

  • October 12, 2024
  • 1 reply
  • 1445 views

Hello all,

I want to use the STM32WB5MMG module for a project which requires an RTC.
The datasheet states the module integrates a 32.774 kHz LSE crystal. That seems a bit strange to me because the standard clock for LSE is normally 32.768 kHz. Checking the reference manual RM0434 there does not seem to be any reference to using a 32.774 kHz clock.

I would like the RTC time to be as accurate as possible, is 32.774 kHz ok to use for the RTC? I guess I would need to somehow offset the faster clock to keep correct time.

Here are some calculations I did, which I have no idea if they are correct.
It seems that a 32.774 kHz clock divided by 2^15 = 1.000183105.

That equals 0.001000183 ms offset from the ideal 1 second per clock period.

Multiply by the number of seconds in a day, 0.001000183×86400 seconds = 86ms offset per day.

If you have any thoughts on the matter, let me know!
Thanks!

-Eric

Best answer by Peter BENSCH

Welcome @EricNava, to the community!

please see the errata ES0525, section 2.1.1 for some more information about this rather unusual 32774Hz crystal.

To get a 1Hz output, you can correct it e.g. using smooth calibration, see RM0434, section 29.4.11.

Hope this helps?

Regards
/Peter

1 reply

Peter BENSCH
Peter BENSCHBest answer
Technical Moderator
October 12, 2024

Welcome @EricNava, to the community!

please see the errata ES0525, section 2.1.1 for some more information about this rather unusual 32774Hz crystal.

To get a 1Hz output, you can correct it e.g. using smooth calibration, see RM0434, section 29.4.11.

Hope this helps?

Regards
/Peter

EricNavaAuthor
Associate II
October 12, 2024

Hi Peter,

Thank you for pointing that out, I should have thought to look at the errata. I guess to use the RTC with the LSE, I will need to do a calibration with the module's 1Hz or 512Hz output.

Thanks for you help

 

 

Peter BENSCH
Technical Moderator
October 12, 2024

I changed my previous comment while you are replying: you can correct the deviation of 183ppm via Smooth Calibration.