STM32WBA BLE Data Throughput example : throughput optimization
Hello everyone,
I'm currently working with the STM32WBA65RI Nucleo board.
For my upcoming application, I require a stable BLE throughput of over 800 kbps. However, using the provided example, I can only achieve around 600 kbps.
So far:
I'm using an MTU of 244 bytes.
- 2M PHY
Manage to minimize connection interval : 11.25 ms when using the ST BLE Toolbox app, and 7.5 ms when using a custom script on Windows.
I’ve tested with several smartphones/ configuration and also tried increasing the MCU clock, but none of these changes improved the performance significantly.
Has anyone managed to achieve a higher throughput with this setup or found effective optimizations?
Thanks in advance for any insights.