STM32WBA65RI BLE Advertise with Standby Mode
Hello,
I am currently working with the NUCLEO-STM32WBA65RI. My main goal is to place the board in Standby mode and periodically wake it up to perform BLE advertising (as a Peripheral), while still allowing it to handle a possible connection request from another device.
So far, I have followed the "Standby with RTC" example to implement low-power operation. I would now like to integrate the BLE stack to enable advertising during the wake-up periods. The intended behavior is for the device to sleep for 1 minute, wake up via the RTC, perform advertising for a short duration, and then return to Standby mode.
From the documentation, I understand that the radio and Link Layer must be in deep sleep for Standby mode to be properly achieved. Could you provide some guidance on the correct way to ensure this state? Additionally, what happens if the radio is not in deep sleep when attempting to enter Standby mode?
Best regards,