STM32WL Maximum storage temperature
I have an unusual question. The storage temperature range for an STM32WL is stated as: -65 to +150 °C.
We are looking at doing some particular tests at high temperatures for radiation exposure recovery, so some questions if anyone knows:
1. If we put the chips in an oven at 140 °C, powered off, for 6 months is there a likely hood of FLASH data loss ?
2. If the FLASH does lose data, I assume some factory settings could also be lost ?
3. Is it possible to reprogram the factory settings and the internal ROM code if this gets messed up ?
4. Would the STM32 still be accessible via the SWD interface even if the internal settings/FLASH is messed up ?