STM32WL5 Radio Init
Hello, sorry to waste your time, but I don't understand. I use a NUCLEO-WL55JC1, after some test with the example in the WL_Package, and some errors to adaptate the example code. I have undertaken to start from zero. I use the example code in the Mono Core Ping Pong example, but I don't use the sequencer (not very usefull in my case). So :
I wan't to send data every x seconds, for this I use TIM2. In the TIM_IRQ I have to toggle pin (work) and send data (don't work). To test if I can send data, I check if I have "TxDone" or "TxTimeout" (nope) and I use a 2nd WL55C1 with a working code in Rx mode to check if I receive something (nope). So clearly :
TIM2 -> Working
Radio -> Not working
USART2 -> Working
USART1 -> Not implemented
I check multiple times my init of subghz, and I think I have all I need. I upload the "subghz_phy_app" and "TIM2_IRQHandler" code. Clearly I miss something, but what ? I already check if I call "subghz_init" and yes. Can you help me pls ?
void TIM2_IRQHandler(void)
{
/* USER IRQ CODE BEGIN */
isMaster = ((GPIOC->IDR >> 4) & 1);
if (!isMaster)
{
Radio.Rx(3000);
} else
{
HAL_Delay(Radio.GetWakeupTime());
HAL_GPIO_TogglePin(LED1_GPIO_Port, LED1_Pin);
HAL_UART_Transmit(&huart2, (uint8_t *)"IRQ Tx\r\n", 8, 1000);
radio_status_t status = Radio.Send((uint8_t *)"Test", 64);
if(status == (radio_status_t)"OK")
{
HAL_UART_Transmit(&huart2, (uint8_t *)"OK Tx\r\n", 7, 1000);
} else if (status == (radio_status_t)"ERROR")
{
HAL_UART_Transmit(&huart2, (uint8_t *)"ERROR Tx\r\n", 10, 1000);
} else
{
HAL_UART_Transmit(&huart2, (uint8_t *)"NONE Tx\r\n", 9, 1000);
}
}
/* USER IRQ CODE END */
//reset the interrupt flag
TIM2->SR = (0 << 0);
}
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file subghz_phy_app.c
* @author MCD Application Team
* @brief Application of the SubGHz_Phy Middleware
******************************************************************************
* @attention
*
* Copyright (c) 2024 STMicroelectronics.
* All rights reserved.
*
* This software is licensed under terms that can be found in the LICENSE file
* in the root directory of this software component.
* If no LICENSE file comes with this software, it is provided AS-IS.
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "platform.h"
#include "sys_app.h"
#include "subghz_phy_app.h"
#include "radio.h"
/* USER CODE BEGIN Includes */
#include "usart.h"
/* USER CODE END Includes */
/* External variables ---------------------------------------------------------*/
/* USER CODE BEGIN EV */
/* USER CODE END EV */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define RF_FREQUENCY 868000000 /* Hz */
#define TX_OUTPUT_POWER 14 /* dBm */
#define LORA_BANDWIDTH 0 /* [0: 125 kHz, 1: 250 kHz, 2: 500 kHz, 3: Reserved] */
#define LORA_SPREADING_FACTOR 7 /* [SF7..SF12] */
#define LORA_CODINGRATE 1 /* [1: 4/5, 2: 4/6, 3: 4/7, 4: 4/8] */
#define LORA_PREAMBLE_LENGTH 8 /* Same for Tx and Rx */
#define LORA_SYMBOL_TIMEOUT 5 /* Symbols */
#define LORA_FIX_LENGTH_PAYLOAD_ON false
#define LORA_IQ_INVERSION_ON false
#define PAYLOAD_LEN 64
#define TX_TIMEOUT_VALUE 3000
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
/* Radio events function pointer */
static RadioEvents_t RadioEvents;
/* USER CODE BEGIN PV */
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
/*!
* @brief Function to be executed on Radio Tx Done event
*/
static void OnTxDone(void);
/**
* @brief Function to be executed on Radio Rx Done event
* @PAram payload ptr of buffer received
* @PAram size buffer size
* @PAram rssi
* @PAram LoraSnr_FskCfo
*/
static void OnRxDone(uint8_t *payload, uint16_t size, int16_t rssi, int8_t LoraSnr_FskCfo);
/**
* @brief Function executed on Radio Tx Timeout event
*/
static void OnTxTimeout(void);
/**
* @brief Function executed on Radio Rx Timeout event
*/
static void OnRxTimeout(void);
/**
* @brief Function executed on Radio Rx Error event
*/
static void OnRxError(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Exported functions ---------------------------------------------------------*/
void SubghzApp_Init(void)
{
/* USER CODE BEGIN SubghzApp_Init_1 */
/* USER CODE END SubghzApp_Init_1 */
/* Radio initialization */
RadioEvents.TxDone = OnTxDone;
RadioEvents.RxDone = OnRxDone;
RadioEvents.TxTimeout = OnTxTimeout;
RadioEvents.RxTimeout = OnRxTimeout;
RadioEvents.RxError = OnRxError;
Radio.Init(&RadioEvents);
/* USER CODE BEGIN SubghzApp_Init_2 */
Radio.SetChannel(RF_FREQUENCY);
Radio.SetTxConfig(MODEM_LORA, TX_OUTPUT_POWER, 0, LORA_BANDWIDTH,
LORA_SPREADING_FACTOR, LORA_CODINGRATE,
LORA_PREAMBLE_LENGTH, LORA_FIX_LENGTH_PAYLOAD_ON,
true, 0, 0, LORA_IQ_INVERSION_ON, TX_TIMEOUT_VALUE);
Radio.SetRxConfig(MODEM_LORA, LORA_BANDWIDTH, LORA_SPREADING_FACTOR,
LORA_CODINGRATE, 0, LORA_PREAMBLE_LENGTH,
LORA_SYMBOL_TIMEOUT, LORA_FIX_LENGTH_PAYLOAD_ON,
0, true, 0, 0, LORA_IQ_INVERSION_ON, true);
Radio.SetMaxPayloadLength(MODEM_LORA, PAYLOAD_LEN);
Radio.Rx(RX_TIMEOUT_VALUE);
/* USER CODE END SubghzApp_Init_2 */
}
/* USER CODE BEGIN EF */
/* USER CODE END EF */
/* Private functions ---------------------------------------------------------*/
static void OnTxDone(void)
{
/* USER CODE BEGIN OnTxDone */
HAL_UART_Transmit(&huart2, (uint8_t *)"TxDone\r\n", 8, 1000);
/* USER CODE END OnTxDone */
}
static void OnRxDone(uint8_t *payload, uint16_t size, int16_t rssi, int8_t LoraSnr_FskCfo)
{
/* USER CODE BEGIN OnRxDone */
HAL_UART_Transmit(&huart2, (uint8_t *)"RxDone\r\n", 8, 1000);
/* USER CODE END OnRxDone */
}
static void OnTxTimeout(void)
{
/* USER CODE BEGIN OnTxTimeout */
HAL_UART_Transmit(&huart2, (uint8_t *)"TxTimeout\r\n", 11, 1000);
/* USER CODE END OnTxTimeout */
}
static void OnRxTimeout(void)
{
/* USER CODE BEGIN OnRxTimeout */
HAL_UART_Transmit(&huart2, (uint8_t *)"RxTimeout\r\n", 11, 1000);
/* USER CODE END OnRxTimeout */
}
static void OnRxError(void)
{
/* USER CODE BEGIN OnRxError */
HAL_UART_Transmit(&huart2, (uint8_t *)"RxError\r\n", 9, 1000);
/* USER CODE END OnRxError */
}
/* USER CODE BEGIN PrFD */
/* USER CODE END PrFD */