STM32WL55 LoRAWAN Live object can't join
Hello everyone,
I am trying to communicate via LoRaWAN on the live object network of the French operator Orange. I'm using the nucleo STM32WL55 for the end device.
Here are the version of the application on the end device side :
APPLICATION_VERSION: V1.3.1
MW_LORAWAN_VERSION: V2.6.1
MW_RADIO_VERSION: V1.3.1
L2_SPEC_VERSION: V1.0.3
RP_SPEC_VERSION: V1-1.0.3
I tried with these two lora mac version :
I think the problem come from a configuration.
Do you guys have any idea of what the issue ?