Skip to main content
Associate III
August 3, 2025
Question

stm32wle5 bga package - output return loss measurement(tx mode)

  • August 3, 2025
  • 1 reply
  • 304 views

Hi ,

 

I am trying to measure the output return loss ( in tx mode) of my board rf chain which include the stm32wle5.

if i understnad correctly - in order to do that i need to put the STM32WLE5  in TX MODE which means its PA should be powered up and ready to transmit but without any transmitted data.  ( so that i will be able to measure the Return loss using external VNA connected to the TX RF PORT of my board)

is there an option to do that ?  i cant seem to find a way to make the internal PA ready to transmit (powered up) without actually transmitting .   is it possible to measure the output RL as i described ?

 

thank you,

viola

1 reply

STTwo-32
Technical Moderator
September 19, 2025

Hello @viola 

May i know why are you interested in this? Are you experiencing unsatisfactory TX performance that is far from what is stated in the datasheet?

Best Regards.

STTwo-32