Skip to main content
Associate II
February 14, 2025
Solved

STM32WLE5 Module JOIN FAILED

  • February 14, 2025
  • 1 reply
  • 682 views

Hi,

I'm doing tests based on the LoRaWAN_AT_Slave. One of the modules often appears tMAC txTimeOut, resulting in JOIN FAILED. Same firmware downloaded, but some devices are working, is there any doubt? Is it a hardware problem?

 

[14:47:35.933]发→◇AT+JOIN=1
□
[14:47:35.965]收←◆1s890:TX on freq 470900000 Hz at DR 0

OK

[14:47:39.965]收←◆5s893:MAC txTimeOut
+EVT:JOIN FAILED

 

Best answer by ethan2

Hi,

I have finally solved the problem, it is the hardware cause.

Thanks.

1 reply

STTwo-32
Technical Moderator
February 14, 2025

Hello @ethan2 

Could you please provide more details. What is the exact module you are using (a third party module or a module based on your own design), what is the code you are using and all your use case details if possible.

Best Reagards.

STTwo-32

ethan2AuthorBest answer
Associate II
February 21, 2025

Hi,

I have finally solved the problem, it is the hardware cause.

Thanks.