STOP mode and BLE
Hey. I currenlty have a wba55 baord and use it as a ble p2p server. The main idea is to put put the board to stop0/1 mode when disconnected so that it consumes some μ amps and turn it back on when receiving a specific interrupt (eg button, timer etc).
I tried a minimal bare-metal example, where i turned on every peripheral (uart, i2c etc) i would use on my actual project to monitor power consumption and before sleep mode i de-inited each and every one of them and all interrupt sources other than the specific EXTI line. The thing is that the device seemed like unable to even enter stop mode. I turned off the rf module through mx and it worked perfectly.
So from what i understood, the rf module and be in general produces a ton of interrupts which doesn't let the device to stay in stop mode. Is there any way to disable the rf module/ ble during runtime and re enable it once the device wakes up from the intended interrupt source ?