Visitor II
July 30, 2024
Question
SubGhz Ping Pong Dual Core
- July 30, 2024
- 1 reply
- 920 views
Hi All,
We have designed a board using the STM32WL55CCU6 [UQFPN 48 pin] chip and successfully brought it up. We have tested the USART, and it is working correctly. However, when we try to port and run the example of SubGHz Ping Pong Dual Core, it does not work as expected. The program gets halted after calling the function "MX_SubGHz_Phy_Init();". We followed the procedures outlined in the readme file which I had added along with the query. The modifications for the files are done as mentioned in the readme but the switching between the cores is not happening. I am adding a file where the program is halted.

Can anyone provide the correct procedure for this?