Timer TIM2 does not work when BLE is initialized in STM32WB55.
Hello.
I am facing a problem: timer tim2 is not working with initialized ble and tasks and timers HW_TS (button and LED processing). Just in case, I checked that TIM16 is working, but it is busy with another task, so I can't use it. I've tried many things, but all I get is either the interrupt triggering instantly and going to hard fault, or just going to an error handler, or nothing happening.
static void MX_TIM2_Init(void)
{
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 31999;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 2999;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
}If I comment out all the initialization MX_APPE_Init(); and MX_APPE_Process(); then the timer will work.
Please help me solve this problem. Let me know if you need any additional information or code.