Using stm32wb55 without low pass filter?
Is it possible to use stm32wb55 radio without DLF162500? I mean I have nothing to complain about its price but rather that it uses a non standard package/footprint and I don't want to have any non standard components so I can change components so long as they have similar performance but designing a filter with performance similar to this one would be hard out of discrete components.
Also I'm curious why no stm32wb user manual nor datasheet mentions the existence of mlfp-wb55-02E3 and similar, it happens to be as well that the nucleo board uses LFB182G45C which is a band pass filter.... All of these components have the same problem for me which is they don't use standard package/footprint sizes.
All in all can I remove this low pass filter and still have a working bluetooth 5.4 radio?