Skip to main content
Dimitrios Bako
Associate II
October 15, 2024
Solved

W-MBus Example Code for WL55JC1

  • October 15, 2024
  • 1 reply
  • 1165 views

Dear All,

Our work is focused on the STM32 WL55JC1 board!

What we would like to achieve is use its RF transceiver as W-MBus.

It seems that WL55 is suitable for WM-Bus since its transceiver supports the appropriate frequencies and modulations for such purpose.

Still I was not able to find any example code so that WL55 can be used with WM-Bus and trying to do it from scratch seems difficult for someone not that experienced.

Looking at X-CUBE-SUBG1 package there are lots of examples for WM-Bus but they target the SPIRIT1 and S2-LP transceivers.

I was thinking to manually integrate the WM-Bus example code (X-CUBE-SUBG1) to WL55 but I guess it will not work out-of-the-box since it is equipped with another transceiver (I think Semtech).

I wanted to ask if anyone is aware of an example code to use WM-Bus with WL55 or if anyone can provide a suggestion/help to this direction!

 

Thank you!

Best answer by STTwo-32

Hello @Dimitrios Bako 

the Wireless M-Bus for the STM32WL is available from our partner StackForce as a commercial version only, as you can find on their website.

Best Regards.

STTwo-32

1 reply

STTwo-32
STTwo-32Best answer
Technical Moderator
October 15, 2024

Hello @Dimitrios Bako 

the Wireless M-Bus for the STM32WL is available from our partner StackForce as a commercial version only, as you can find on their website.

Best Regards.

STTwo-32

Dimitrios Bako
Associate II
October 15, 2024

Dear STTwo-32,

Thank you very much for the quick reply!

Best regards,

Dimitrios Bakoyiannis