WB55: Can BLE_Zigbee_Static enter Stop2 mode?
Hello,
I am using Nucleo-64 to evaluate the Zigbee power consumption of WB55. When testing Zigbee, it can be seen that after adding Zigbee, the power consumption of the development board is significantly reduced, and the measured average current does not exceed 500ua.
However, when testing the BLEZigbee_Static routine, even after the addition was completed, the current did not significantly decrease and remained greater than 10ma. And I couldn't find any explanation about low power consumption in the readme. txt file.
Based on the above situation, I speculate that BLEZigbee_Static has not entered Stop2 mode. I want to know if it is possible to support both BLE and ZigBee while ensuring low power consumption.
Thank you
Weng