Skip to main content
TLans.1
Associate
July 17, 2024
Solved

WB55RG/WB15CC and PLC01A1

  • July 17, 2024
  • 1 reply
  • 1095 views

Is NUCLEO-WB55RG/WB15CC compatible with X-NUCLEO-PLC01A1?

I want to develop a controller that supports BLE and thought of starting with a combination of these two boards. Would be helpful if someone can confirm that these boards are compatible and can be stacked and work together.

Thanks. 

Best answer by STTwo-32

Hello @TLans.1 

As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.

Best Regards.

STTwo-32

 

1 reply

STTwo-32
STTwo-32Best answer
Technical Moderator
August 13, 2024

Hello @TLans.1 

As we can see on the UM1918, the X-NUCLEO-PLC01A1 can be Plugged onto any STM32 Nucleo board through the Arduino UNO R3 connectors. So, the Shield is Compatible with the NUCLEO-WB55RG/WB15CC that includes the Arduino R3 Connectors.

Best Regards.

STTwo-32