Skip to main content
Associate II
May 9, 2025
Solved

Why is the second "antenna matching network" not shown in the example?

  • May 9, 2025
  • 1 reply
  • 425 views

Hi, 

Im developing stm32wb55ceu6 RF application hardware. In the application note AN5290 it says that a second antenna matching network is needed after the LP filter . But i cant find anything else about this matching network.

siyar_0-1746813340748.png

Next page at the schematic example, this second antenna matching network is not implemented. can someone shed some light on the this topic, thanks in advance.

siyar_1-1746813431320.png

 

 

 

 

Best answer by STTwo-32

Hello @siyar 

For more data about that, I suggest you have a look at this video. It should help you with good explanation. The figures are just stopped after the IPD directly. The second antenna matching is visible only on the full design. So, you have to follow the recommendations of the video and the RF matching paragraph.

Best Regards.

STTwo-32

1 reply

STTwo-32
STTwo-32Best answer
Technical Moderator
May 9, 2025

Hello @siyar 

For more data about that, I suggest you have a look at this video. It should help you with good explanation. The figures are just stopped after the IPD directly. The second antenna matching is visible only on the full design. So, you have to follow the recommendations of the video and the RF matching paragraph.

Best Regards.

STTwo-32