X-NUCLEO-GFX01M2 SPI frequency
Hello,
I am currently using a X-NUCLEO-GFX01M2 screen to display logs from a NUCLEO-STM32WL55JC board. Unfortunately, it is quite slow to display the logs, so I wanted to improve the SPI frequency. I tested it by lowering the SPI BaudRatePrescaler from the nucleo board, but below 16, I noticed no improvements. When measuring the SPI clock, there is no improvement above roughly 3 MHz.
How can I improve the SPI link?
Moreover, there is nothing related to the max SPI frequency in any X-NUCLEO-GFX01M2 documentation. What is the max frequency the GFX01M2 screen can support?
Regards,
Sacha