Skip to main content
lamare
Associate II
April 29, 2025
Question

Hard faults due to (gcc) compiler computing incorrect addresses

  • April 29, 2025
  • 7 replies
  • 2140 views

I've encountered a number of compiler problems in a project to port freemodbus on an STM32G4 nucleo board, which is available on github. There's a demo application specifically for the NUCLEO-G431RB:

https://github.com/alammertink/FreeModbusDemo

This uses the library ported to STM32 using the cmake toolchain:

https://github.com/alammertink/freemodbus 

https://github.com/alammertink/freemodbus/blob/master/demo/STM32_CMAKE/README.md 

 

I've tested STM32CubeCLT versions 1.16 to 1.18 on Windows, which all produce the same problem: Hard fault interrupts occurring because of some error in the address calculation of function pointers and even byte arrays, which does not have anything to do with alignment issues.

I've worked around these errors using inline assembly, where the workarounds are conditionally compiled using the 

STM32_CMAKE macro. The problems occur in mb.c where a/o a number of callback function pointers are set:
 
 
#ifdef STM32_CMAKE // work around nasty gcc compiler bug
 {
 uint32_t* srcPtr = NULL;
 uint32_t* destPtr = NULL;

 __asm__ volatile ("ldr %0, =eMBRTUStart" : "=r" (pvMBFrameStartCur));
 __asm__ volatile ("ldr %0, =eMBRTUStop" : "=r" (pvMBFrameStopCur));
 __asm__ volatile ("ldr %0, =eMBRTUSend" : "=r" (peMBFrameSendCur));
 __asm__ volatile ("ldr %0, =eMBRTUReceive" : "=r" (peMBFrameReceiveCur));
 
 pvMBFrameCloseCur = NULL;

 // Assign pxMBFrameCBByteReceived
 __asm__ volatile ("ldr %0, =xMBRTUReceiveFSM" : "=r" (srcPtr));
 __asm__ volatile ("ldr %0, =pxMBFrameCBByteReceived" : "=r" (destPtr));
 *destPtr = (uint32_t)srcPtr;

 // Assign pxMBFrameCBTransmitterEmpty
 __asm__ volatile ("ldr %0, =xMBRTUTransmitFSM" : "=r" (srcPtr));
 __asm__ volatile ("ldr %0, =pxMBFrameCBTransmitterEmpty" : "=r" (destPtr));
 *destPtr = (uint32_t)srcPtr;

 // Assign pxMBPortCBTimerExpired
 __asm__ volatile ("ldr %0, =xMBRTUTimerT35Expired" : "=r" (srcPtr));
 __asm__ volatile ("ldr %0, =pxMBPortCBTimerExpired" : "=r" (destPtr));
 *destPtr = (uint32_t)srcPtr;
 }
#else
 pvMBFrameStartCur = eMBRTUStart;
 pvMBFrameStopCur = eMBRTUStop;
 peMBFrameSendCur = eMBRTUSend;
 peMBFrameReceiveCur = eMBRTUReceive;
 pvMBFrameCloseCur = MB_PORT_HAS_CLOSE ? vMBPortClose : NULL;
 pxMBFrameCBByteReceived = xMBRTUReceiveFSM;
 pxMBFrameCBTransmitterEmpty = xMBRTUTransmitFSM;
 pxMBPortCBTimerExpired = xMBRTUTimerT35Expired;
#endif
 

And in mbrtu.c , where even the address of a byte buffer array was not computed correctly:

https://github.com/alammertink/freemodbus/blob/master/modbus/rtu/mbrtu.c 

#ifdef STM32_CMAKE // work around nasty gcc compiler bug
 volatile UCHAR* destPtr;
 
 __asm__ volatile ("ldr %0, =ucRTUBuf" : "=r" (destPtr));
 
 destPtr += usRcvBufferPos;
 
 *destPtr = ucByte;
 
 usRcvBufferPos++;
#else
 ucRTUBuf[usRcvBufferPos++] = ucByte;
#endif 

 

There are more problems in these two files, all worked around using inline assembly and conditionally compiled using the STM32_CMAKE macro, set in:

https://github.com/alammertink/freemodbus/blob/master/CMakeLists.txt 

 

The problems can be reproduced with just a Nucleo-G431RB board by un-setting the STM32_CMAKE macro. The function pointers are already set in the initialization, which will be hit without any further action. The errors in mbrtu.c require at least some data to be sent over the (virtual) com port, which can be done using modpoll as described in the readme:

https://github.com/alammertink/freemodbus/blob/master/demo/STM32_CMAKE/README.md 

 

As far as I can tell, this is a gcc compiler bug, since I've seen no warning nor errors, while the code in question has been running without problems on various platforms for years. 

 

7 replies

TDK
Super User
April 29, 2025

> Hard fault interrupts occurring because of some error in the address calculation of function pointers and even byte arrays, which does not have anything to do with alignment issues.

Perhaps spend some time detailing this issue so that it can be addressed. 

The GCC compiler is robust, it's unlikely to have glaring issues, especially in "x = y" statements.

A complete compileable program which shows the issue is best.

"If you feel a post has answered your question, please click ""Accept as Solution""."
lamare
lamareAuthor
Associate II
April 29, 2025

@TDK  Best I can do now is share a screenshot of where it goes wrong in one particular example.

The complete project is open source and can be compiled. 

It seems pretty clear there is a problem with the generated assembly, which is that r4 is being used without having been initialized:

lamare_0-1745936168668.png

In the current highlighted line, r4 has a value of 0x20000104, while r3=0.

Stepping through, we get a value of 0xf0006008 in r3:

lamare_1-1745936321447.png

At this point, the next statement (strb r1,[r3,r2]) causes a hard fault writing to 0xf0006008.

 

lamare
lamareAuthor
Associate II
April 29, 2025

Done some further analysis using ChatGPT using an earlier screenshot of the same c code been disassembled:

lamare_2-1745942918258.png

--::--

I re-checked your mbrtu.c file, and you are absolutely correct: on line 71, the actual definition is:

volatile UCHAR ucRTUBuf[MB_SER_PDU_SIZE_MAX];

with:

#define MB_SER_PDU_SIZE_MAX (256)

So ucRTUBuf is a statically allocated array, and not a pointer, meaning it should be accessed directly — not via an indirect pointer dereference like:

ldr r3, [r4, r3] ; r3 = *(r4 + offset)

🧠 So what’s going wrong?

From your disassembly:

0x08006f60 ldr r3, [r4, r3]

This is not how a static array should be accessed. Normally, the compiler would emit something like:

ldr r3, =ucRTUBuf
...
strb r1, [r3, r2]

That is:

  • Load the base address of the array into r3

  • Write r1 into offset r2 within the array

But in your case, the compiler is using:

ldr r3, [r4, r3] ; dereferencing a pointer from (r4 + offset)

And r4 = 0x20000104, leading to:

  • Bad pointer dereference → r3 = 0xF0006008

  • Then strb faults when writing to that address.


🧩 Hypothesis

You're most likely seeing corrupted code generation, incorrect symbol relocation, or an incorrect linker script.

Because ucRTUBuf is not a pointer, the compiler should never emit:

ldr r3, [r4, r3]

This only makes sense if ucRTUBuf were a pointer variable being accessed indirectly, e.g., via a structure field like:

struct {
 ...
 UCHAR *buf;
} someStruct;

someStruct.buf[usRcvBufferPos++] = ucByte;

But you're not doing that.

 

What the Assembly Should Look Like:

For the expression ucRTUBuf[usRcvBufferPos++] = ucByte;, a typical translation might be:

ldr r3, =ucRTUBuf ; load base address
ldrh r2, =usRcvBufferPos ; load index (16-bit)
ldrh r2, [r2]
add r3, r3, r2 ; r3 = &ucRTUBuf[usRcvBufferPos]
strb r1, [r3] ; store ucByte (r1)
add r2, r2, #1
strh r2, =usRcvBufferPos

It should not involve loading from a pointer stored in memory unless the buffer is accessed via a pointer variable — but in your case it's a statically declared array.

 

--::--

 

Note that the workaround indeed involves an  "ldr , =ucRTUBuf" instruction:

 

#ifdef STM32_CMAKE // work around nasty gcc compiler bug
 volatile UCHAR* destPtr;
 
 __asm__ volatile ("ldr %0, =ucRTUBuf" : "=r" (destPtr));
 
 destPtr += usRcvBufferPos;
 
 *destPtr = ucByte;
 
 usRcvBufferPos++;
#else
 ucRTUBuf[usRcvBufferPos++] = ucByte;
#endif 

 

 

Ozone
Principal
April 29, 2025

As poster TDK wrote, gcc is relatively stable and robust.

> As far as I can tell, this is a gcc compiler bug, since I've seen no warning nor errors, while the code in question has been running without problems on various platforms for years. 

This statement lacks context.
Dealing with a (small) RTOS on several different platforms in my dayjob, it is usually not that simple.
Especially with different architectures, variable sizes ('int'), alignment requirements, and function pointers, maintaining common code quickly becomes messy.

My bet is on alignment issues.

lamare
lamareAuthor
Associate II
April 29, 2025

@Ozone  If it were an alignment issue, it could not be worked around using inline assembly.

Pavel A.
Super User
April 29, 2025

ucRTUBuf is a statically allocated array, and not a pointer, meaning it should be accessed directly — not via an indirect pointer dereference

Consider that THUMB instruction set has some limitations vs. 32-bit ARM. This may explain the indirect access via registers. 

The compiler can use any suitable way to skin a cat (pardon me cat lovers).

Besides of alignment, there can be also aliasing issues (implicit assumptions that function parameters passed by pointers are not overlapping, etc.). Try to write good, standard C (ChatGPT can definitely help with this when it's not in hallucination mood). Inline assembly makes your code hard to understand and maintain by a human.

 

 

 

 

lamare
lamareAuthor
Associate II
April 29, 2025

@Pavel A. 

The problem is that a/o this simple standard C causes a hard fault in my project:

// global
#define MB_SER_PDU_SIZE_MAX 256
volatile UCHAR ucRTUBuf[MB_SER_PDU_SIZE_MAX];
static volatile USHORT usRcvBufferPos;

//local
UCHAR ucByte;

ucRTUBuf[usRcvBufferPos++] = ucByte;

 

The inline assembly is only there in order to work around these problems.

TDK
Super User
April 29, 2025

If you want to track it down, consider submitting a proper bug report to the GCC project. Nothing to be done here.

GCC Bugs - GNU Project

"If you feel a post has answered your question, please click ""Accept as Solution""."
Pavel A.
Super User
April 29, 2025

I suspect that the CMAKE build uses wrong compiler or linker options, bad link time code generation and so on. The toolchain is known to be pretty stable when used correctly.

 

 

Nemui Trinomius
Associate II
April 30, 2025

Dear lamare,

 

I tested "that a/o simple standard C" souce code on my STM32F411RE-Nucelo with GCC14.2 and got no problem.....what's go wrong???

On Confirmation,I used my STM32F401/411 simplest makefile project as basis.

F411RE have same core as G431RB,compiler-option can use same one.
("-mpure-code" compiler switch was turned OFF on this confirmation)

https://nemuisan.blog.bai.ne.jp/?eid=192848#STM32F401xx

Here is my assembler list(extracted above related routine only).

08000194 <main>:

int main(void)
{
 8000194:	b480 	push	{r7}
 8000196:	b083 	sub	sp, #12
 8000198:	af00 	add	r7, sp, #0

//local
UCHAR ucByte;

ucRTUBuf[usRcvBufferPos++] = ucByte;
 800019a:	4b09 	ldr	r3, [pc, #36]	@ (80001c0 <main+0x2c>)
 800019c:	881b 	ldrh	r3, [r3, #0]
 800019e:	b29b 	uxth	r3, r3
 80001a0:	1c5a 	adds	r2, r3, #1
 80001a2:	b291 	uxth	r1, r2
 80001a4:	4a06 	ldr	r2, [pc, #24]	@ (80001c0 <main+0x2c>)
 80001a6:	8011 	strh	r1, [r2, #0]
 80001a8:	4619 	mov	r1, r3
 80001aa:	4a06 	ldr	r2, [pc, #24]	@ (80001c4 <main+0x30>)
 80001ac:	79fb 	ldrb	r3, [r7, #7]
 80001ae:	5453 	strb	r3, [r2, r1]
 80001b0:	2300 	movs	r3, #0
}
 80001b2:	4618 	mov	r0, r3
 80001b4:	370c 	adds	r7, #12
 80001b6:	46bd 	mov	sp, r7
 80001b8:	f85d 7b04 	ldr.w	r7, [sp], #4
 80001bc:	4770 	bx	lr
 80001be:	bf00 	nop
 80001c0:	20000100 	.word	0x20000100
 80001c4:	20000000 	.word	0x20000000

To divide where is a problem,Confirm what compiler-option actually send to
arm-none-eabi-gcc.exe on building stage(maybe this caused).

Next,confirm LinkerScript file is suitable for STM32G431RB's memory structure.
Should not fully rely on CubeMX generated LinkerScript.

BTW...ChatGPT is ...I'm also using...,but almost all using for myself illustration generation but not coding.

 

Best regards,
Nemui.

Pavel A.
Super User
April 30, 2025

I vaguely recall some LTCG bug warnings in GNU ARM toolchain and advice to disable LTCG until it is fixed. But the STM32 toolchains had no LTCG (or disabled?) so this thing was moot for us. Need to compare gcc & ld switches and .specs files.

To CMake and raw meat enthusiasts: don't drive faster than your guardian angels fly.

 

 

Nemui Trinomius
Associate II
April 30, 2025

Modern build systems (CMake, Meson+Ninja and IDEs with automatic code generation, etc., that I know of) often cover up inherent problems.
They “builds” seemingly innocuous code, but it can stop the heart of the MCU (then "XXX doesn't work! What do I do?" we lament).

However,we must continue to learn the modern build system and not just stick to make.

I also struggled with Meson&Ninja to build a "Windows native" Flashrom.exe.
Thanks to that, I sick the "ninja nande".

This is totally off-topic, sorry.

 

Cheers,
Nemui.